cancel
Showing results for 
Search instead for 
Did you mean: 

BUG: STM32CubeIDE Won't connect to ST-LINK v2 debugger on macOS 15.0

KMill
Senior

My setup is macOS 15.0 Sequoia

STM32CubeIDE 1.16.1

STLink-Server v2.1.1

When trying to program or debug a device the following error is shown:

Screenshot 2024-09-19 at 13.00.10.png

Even after re-installing ST-Link server

I have rebooted and re-installed ST-Link Server, but the issue persists.

It's not a show stopper as I can use STM32CubeProgrammer to program the device, on the same machine.

12 REPLIES 12

@pdmazariegos Thanks for the link to that solution on stackoverflow.

I find that it does indeed work. It's a better workaround than the one I came up with!

Hopefully the dev's at ST will be able to get to the bottom of it and push out a compatibiliy release in the near future. I have to keep my macOS up to date for other reasons, so I had no choice but to update to macOS 15.0

@mÆŽALLEm Do you know if ST run a beta programme? I'd be happy to help with beta testing.

*edit* Spelling.

I started ide with the sudo command and it works fine with st-link, macOS 15.1 Intel CPU.

 

This post has been translated from Chinese to comply with the ST Community guidelines.