cancel
Showing results for 
Search instead for 
Did you mean: 

8-bit LCD interfacing

M0nty
Associate II

Hi everyone I'm rather new with programming with STM32 controllers and I am currently using NUCLEO-L432KC. Currently I'm facing a problem with HAL_GPIO_WritePin() function. I am interfacing with a 16x2 LCD and I am trying to write to the RS pin via the function I have mentioned, however I am facing a problem where the RS isn't being set to the desired value I am providing. I have provided the value like so: HAL_GPIO_WritePin(RS_GPIO_Port, RS_Pin, rs);

Where I have given rs = 0 but the function is setting the value as 1. I have also provided the photo of the RS pin configuration from the IOC file.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi

from your ioc file 

PA0.GPIOParameters=GPIO_Label PA0.GPIO_Label=RS PA0.Locked=true PA0.Signal=GPIO_Input

You see the Error? "GPIO_Input"? 

padawan_0-1733211820707.png

padawan

 

View solution in original post

24 REPLIES 24
Andrew Neil
Super User

Welcome to the forum!

 


@M0nty wrote:

Hi everyone I'm rather new with programming with STM32 controllers


Do you have experience with any other microcontroller(s)? With programming in general ?

Please post your source code - instructions here:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

Also your schematic of how the LCD is connected.

A good, clear photo may also help.

Have you checked the Nucleo board's User Manual and/or schematics to see that nothing else is using that pin?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Ghofrane GSOURI
ST Employee

Hello @M0nty 

First let me thank you for posting.

By checking the  HAL_GPIO_WritePin () the parameter :

 

PinState: specifies the value to be written to the selected bit. * This parameter can be one of the GPIO_PinState enum values: * @arg GPIO_PIN_RESET: to clear the port pin * @arg GPIO_PIN_SET: to set the port pin

Ensure that you are passing the correct value for rs. The PinState parameter should be either

GPIO_PIN_SET or GPIO_PIN_RESET, not just 0 or 1. If you are using a variable like rs, make sure

it is defined as:

GPIO_PinState rs = GPIO_PIN_RESET; // or GPIO_PIN_SET

Instead of:

int rs = 0; // This may cause issues

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


@Ghofrane GSOURI wrote:

The PinState parameter should be either GPIO_PIN_SET or GPIO_PIN_RESET, not just 0 or 1.e


The GPIO_PIN_SET and GPIO_PIN_RESET values are 1 and 0 - so it should be OK ...

 

/** * @brief GPIO Bit SET and Bit RESET enumeration */ typedef enum { GPIO_PIN_RESET = 0U, GPIO_PIN_SET }GPIO_PinState;

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mÆŽALLEm
ST Employee

Hello @M0nty and welcome to the community,

Could you please share your ioc file as well as sharing your code?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hello @Andrew Neil 

Let 's just try to use the parameter value as it is GPIO_PIN_SET or GPIO_PIN_RESET and see what's happen.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I have also tried the same thing by substituting rs as GPIO_PIN_RESET but the same issue occurs

No problem, I have provided my ioc file as requested to help you get a better understanding of my configuration

I am actually passing rs as an argument from a function call as shown so I'm not sure if this also causes a problem. (Edit: I tried changing the type of argument for rs from int to GPIO_PinState: void send_cmd(char data, GPIO_PinState rs) but this also doesn't work and the same problem occurs.

 

send_cmd(0x38,0); void send_cmd (char data, int rs) { HAL_GPIO_WritePin(RS_GPIO_Port, RS_Pin, rs); }

 

.  

Time to go back to basics.

Disconnect the LCD.

Go back to a basic "blinky" program which just toggles the LED on the Nucleo board - just a loop with inline delays.

Once that is working, change it to toggle your RS pin.

Does the pin toggle?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.