2025-05-16 10:04 PM
Hi,
I am trying to interface on board microphone in STM32H757I-EVAL. I am trying to use PDM format data. In STM32 Cube IDE, I am trying to configure PE2 as PDM_CLK but it is not listed in the pin configuration. I have attached the image.
2025-05-17 2:14 AM
Hello @priya_12
For the PDM bitstream clock, they are called SAIx_CKy avec X=1 or 4 depending on the SAI interface that you are using and y=[1:4].more details available on the table 445 of the RM0399 rev4.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.