cancel
Showing results for 
Search instead for 
Did you mean: 

VS Code (STM32 Extension) blocks MCU-Finder from starting (Mac OS M1)

TheBigKahuna
Associate II

Just installed the STM32 Extension to VS Code.  If I start the MCU-Finder from within the extension, the MCU banner appears and then hangs in that state.  If I quit VS Code while the MCU Finder banner is visible, the MCU Finder will then continue loading and then open.

The MCU Selector also hangs within STM32CubeMX. If I quit VS Code, the MCU selector will open.

 Any ideas?

I have STM32CubeCLT, STM32CubeMX (6.9.1) , and STMCUFinder (6.0.0) installed.  Mac OS 12.6.8 (M1).

Thanks

2 REPLIES 2
Remyhx
Associate II

I seem to have a similar problem. When I choose “create a new application” from within vscode (stm extension), stm32cubemx starts but hangs on the start my project… choices. Running outside of the extension it just runs. 

ACapo.1
Senior

Still not fixed!

st-stm32cubeclt_1.15.0_20695_20240315_1429-macosx_x86_64.pkg is still not signed!

Stm32CubeMX needs full disk access to run even though it runs fine in STM32Ide.

All in all it is just really poor.