2024-05-24 03:39 AM
When working in remote connections, such as WSL or docker the STM32 extension can not be activated with the following error:
"Cannot activate the 'STM32 VS Code Extension' extension because it depends on the 'C/C++ Extension Pack' extension, which is not loaded. Would you like to reload the window to load the extension?"
But the C/C++ extension is loaded and working.
Is there any Work Around available?
Solved! Go to Solution.
2024-10-29 02:28 AM - edited 2024-10-29 02:29 AM
Suggested Workaround:
"remote.extensionKind": {
"stmicroelectronics.stm32-vscode-extension": [
"workspace"
]
}
Hope this helps!
2024-06-06 01:26 AM
hi @MAdle.1
we are already checking this issue
2024-07-20 07:17 AM
Any updates on this? I'm seeing it with latest version.
2024-07-22 01:25 AM - edited 2024-07-22 01:27 AM
Hi @dmainz
still working on it not yet fixed
but I invite you to check this post it may help you as a workaround
2024-10-18 03:34 AM
Hi @Nawres GHARBI,
is there a solution coming, or does this issue doesn't have any priority?
2024-10-18 04:04 AM
Hello together, hello @Nawres GHARBI
with the help of https://community.st.com/t5/stm32-vscode-extension-mcus/stm32-vs-code-extension-and-devcontainer/td-p/659247/page/2 I found a solution which works for me.
My setup I'm running a devcontainer inside WSL, so the remote connection is windows -> wsl -> devcontainer. For me it seems that the STM32 VSCode must run in the devcontainer and must be disabled in the local installation (like some other extensions). There are two problems, first the extension itself doesn't give the opportunity to install it anywhere else than in the local installation (windows). To get around the issue you have install it locally and then press the cloud symbol on the dev container section in the Extension Tab. Then you can select the STM32 extension to installed in the devcontainer.
The second issue is that, the that instance which is locally installed is not disabled, instead it is still the main instance searching for c++ extension, which locally disabled and enabled in the devcontainer. A solution is now do uninstall the STM32 extension locally. After that reload the vscode and the extension should work in the devcontainer.
I hope this helps finding a solution to get the extension working out of the box.
2024-10-29 02:28 AM - edited 2024-10-29 02:29 AM
Suggested Workaround:
"remote.extensionKind": {
"stmicroelectronics.stm32-vscode-extension": [
"workspace"
]
}
Hope this helps!
2025-01-08 12:55 AM