cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 VS Code Extension Remote Connection

MAdle.1
Associate

When working in remote connections, such as WSL or docker the STM32 extension can not be activated with the following error:
"Cannot activate the 'STM32 VS Code Extension' extension because it depends on the 'C/C++ Extension Pack' extension, which is not loaded. Would you like to reload the window to load the extension?"

But the C/C++ extension is loaded and working.

Is there any Work Around available?

3 REPLIES 3
Nawres GHARBI
ST Employee

hi @MAdle.1 

we are already checking this issue

Any updates on this? I'm seeing it with latest version.

Nawres GHARBI
ST Employee

Hi @dmainz  

still working on it not yet fixed

but I invite you to check this post it may help you as a workaround 

https://community.st.com/t5/stm32-vscode-extension-mcus/stm32-vs-code-extension-and-devcontainer/td-p/659247/page/2