STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 440 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 323 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Reading and writing RAM via ST-Link

I am using STM32MP153 MPU on custom board.Is it possible to read/write memory region using ST-Link connected via JTAG interface?Most interesting if this is possible through some command line interface, perhaps my own C program using some API.

axel101 by Associate III
  • 5464 Views
  • 6 replies
  • 0 kudos

STM32MP157 in KEIL error.

Hello.I use a board STM32MP157A-DK1. I have SD-card with linux and now i try to run the board in KEIL. I have read file "Using STM32MP1 Cortex-M with Keil MDK". But I get error:Error: flash download failed.Also a can see:Full ship erase done.No Algor...

DFomi.1 by Associate II
  • 7691 Views
  • 14 replies
  • 0 kudos

Wrong partition size and "Error while reading the file" while programming flash layout to STM32MP157

Hi,after changing some kernel settings probably, I suddenly can not flash it to our custom STM32MP157 based board. Process fails around 100% of last partition with error: "Error: Error while reading the file"Looks like Cube reads file size incorrectl...

Modify debug load mode of stm32mp157f-dk2

I am using stm32mp157f-dk2 and followed https://wiki.st.com/stm32mpu/wiki/Getting_started with help of stmcubeIDE. I am able to debug M4 core and also see SWV prints with ST A7 image and M4 image. Both images are available through above ST web site. ...

_legacyfs_online_stmicro_images_0693W00000bjxDbQAI.png _legacyfs_online_stmicro_images_0693W00000bjxC9QAI.png _legacyfs_online_stmicro_images_0693W00000bjxCsQAI.png _legacyfs_online_stmicro_images_0693W00000bjxEFQAY.png
Kalpesh1 by Associate II
  • 2768 Views
  • 4 replies
  • 0 kudos