cancel
Showing results for 
Search instead for 
Did you mean: 

When I use bitbake PermissionError: [Errno 13] Permission denied: '/home/dev' error occurs

Gencay
Associate III

I've changed the ownership of the /usr/lib/python3.8 file from root to <myname> but did not solved the problem. Here is the whole error:

ERROR: Command execution failed: Traceback (most recent call last):

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/command.py", line 126, in runAsyncCommand

   commandmethod(self.cmds_async, self, options)

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/command.py", line 607, in buildTargets

   command.cooker.buildTargets(pkgs_to_build, task)

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/cooker.py", line 1581, in buildTargets

   rq = bb.runqueue.RunQueue(self, self.data, self.recipecaches, taskdata, runlist)

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/runqueue.py", line 1229, in __init__

   self.dm = monitordisk.diskMonitor(cfgData)

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/monitordisk.py", line 176, in __init__

   self.devDict = getDiskData(BBDirs)

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/monitordisk.py", line 121, in getDiskData

   bb.utils.mkdirhier(path)

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/utils.py", line 740, in mkdirhier

   raise e

 File "/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/bitbake/lib/bb/utils.py", line 737, in mkdirhier

   os.makedirs(directory)

 File "/usr/lib/python3.8/os.py", line 213, in makedirs

   makedirs(head, exist_ok=exist_ok)

 File "/usr/lib/python3.8/os.py", line 223, in makedirs

   mkdir(name, mode)

PermissionError: [Errno 13] Permission denied: '/home/dev'

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Gencay
Associate III

My problem was misconfigurations of my download, sstate-cache and tmp directories at the local.conf file.

View solution in original post

4 REPLIES 4
Kevin HUBER
ST Employee

Hello @Gencay​ ,

Please can you send me the command line that you are trying to use?

On which Operating System are you? Can you make a "lsb_release -a" and send me the result.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Gencay
Associate III

Distributor ID:   Ubuntu

Description:   Ubuntu 20.04.4 LTS

Release:   20.04

Codename:   focal

the command line I am using is bitbake st-image-core

Gencay
Associate III

My problem was misconfigurations of my download, sstate-cache and tmp directories at the local.conf file.