Skip to main content
zxiao.4
Associate III
August 1, 2022
Solved

Hi: I'm using st-image-weston-openstlinux-weston-stm32mp1.ext4. The USB mouse works, but the touch screen doesn't respond.

  • August 1, 2022
  • 7 replies
  • 3679 views

Using hexdump /dev/input/event1, you can see the data changes. when I use ts_ test command, "open fbdevice: no such file or directory" will appear. Please help me, I really don't know how to configure it.I am sure that the touch screen monitoring is correct and the data is uploaded correctly.

This topic has been closed for replies.
Best answer by zxiao.4

I've fixed it. It should be the problem of touch coordinates. I just rotate in the device tree and reverse direction.

7 replies

Gregory PLANCHON
ST Technical Moderator
August 4, 2022

Hi @zxiao.4​ ,

I need additional information in order to find the problem.

Can you tell me which card you use and which version of openstlinux ?

What did you do for the moment ? 

Did you follow the distribution package ?

regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
zxiao.4
zxiao.4Author
Associate III
August 5, 2022

Hi:

I use a customized board, similar to stm32mp157d-dk1. Opstlinux 5.15.04 kernel. The error log of Weston is as follows:​

read-back format: BGRA

        EGL Wayland extension: yes

[13:49:56.022] event0 - gpio-keys: is tagged by udev as: Keyboard

[13:49:56.022] event0 - gpio-keys: device is a keyboard

[13:49:56.050] event1 - generic ft5x06 (82): is tagged by udev as: Touchscreen

[13:49:56.056] event1 - generic ft5x06 (82): device is a touch device

[13:49:56.264] libinput: configuring device "gpio-keys".

[13:49:56.265] Touchscreen - generic ft5x06 (82) - /sys/devices/platform/soc/40013000.i2c/i2c-1/1-0038/input/input1/event1

[13:49:56.265] libinput: configuring device "generic ft5x06 (82)".

[13:49:56.265] input device event1 has no enabled output associated (none named), skipping calibration for now.

[13:49:56.265] DRM: head 'DPI-1' updated, connector 32 is connected, EDID make 'unknown', model 'unknown', serial 'unknown'

[13:49:56.266] DRM: head 'DPI-1' found, connector 32 is connected, EDID make 'unknown', model 'unknown', serial 'unknown'

[13:49:56.267] Registered plugin API 'weston_drm_output_api_v1' of size 12

[13:49:56.267] Color manager: no-op

[13:49:56.268] Output 'DPI-1' using color profile: built-in default sRGB SDR profile

[13:49:56.307] Chosen EGL config details: id: 11 rgba: 8 8 8 0 buf: 24 dep: 0 stcl: 0 int: 1-60 type: win|pix|pbf|swap_preserved vis_id: XRGB8888 (0x34325258)

[13:49:56.307] Output DPI-1 (crtc 37) video modes:

        1024x600@60.0, preferred, current, 51.2 MHz

[13:49:56.308] associating input device event0 with output DPI-1 (none by udev)

[13:49:56.308] associating input device event1 with output DPI-1 (none by udev)

[13:49:56.310] Output 'DPI-1' enabled with head(s) DPI-1

[13:49:56.310] Compositor capabilities:

        arbitrary surface rotation: yes

        screen capture uses y-flip: yes

        cursor planes: yes

        arbitrary resolutions: no

        view mask clipping: yes

        explicit sync: yes

        color operations: no

        presentation clock: CLOCK_MONOTONIC, id 1

        presentation clock resolution: 0.000000001 s

[13:49:56.315] Loading module '/usr/lib/weston/desktop-shell.so'

[13:49:56.331] launching '/usr/libexec/weston-keyboard'

[13:49:56.336] Warning: support for deprecated wl_shell interface is enabled. Please migrate legacy clients to xdg-shell.

[13:49:56.339] Loading module '/usr/lib/weston/systemd-notify.so'

[13:49:56.341] launching '/usr/libexec/weston-desktop-shell'

zxiao.4
zxiao.4Author
Associate III
August 5, 2022

input device event1 has no enabled output associated (none named), skipping calibration for now.

​

I think this should be the reason for the mistake, but I don't know how to correct it.

Gregory PLANCHON
ST Technical Moderator
August 5, 2022

Hello,

Could you share me your device tree In order to check if the I2C is well configured.

regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
zxiao.4
zxiao.4Author
Associate III
August 5, 2022

&i2c2 {

    ft5x06: ft5x06@38 {

        compatible = "edt,edt-ft5x06","edt,edt-ft5406";

        interrupt-parent = <&gpioi>;

        interrupts = <1 IRQ_TYPE_EDGE_FALLING>; /* TOUCH_INT# */

        vcc-supply = <&v3v3>;

        reg = <0x38>;

        reset-gpios = <&gpioh 15 GPIO_ACTIVE_LOW>;  /* TOUCH_RESET# */

        touchscreen-size-x = <1024>;

        touchscreen-size-y = <600>;

        status = "okay";

    };

};

​

root@stm32mp1:~# evtest

No device specified, trying to scan all of /dev/input/event*

Available devices:

/dev/input/event0:   gpio-keys

/dev/input/event1:   generic ft5x06 (82)

Select the device event number [0-1]: 1

Input driver version is 1.0.1

Input device ID: bus 0x18 vendor 0x0 product 0x0 version 0x0

Input device name: "generic ft5x06 (82)"

Supported events:

 Event type 0 (EV_SYN)

 Event type 1 (EV_KEY)

  Event code 330 (BTN_TOUCH)

 Event type 3 (EV_ABS)

  Event code 0 (ABS_X)

   Value  574

   Min    0

   Max   1023

  Event code 1 (ABS_Y)

   Value   70

   Min    0

   Max   599

  Event code 47 (ABS_MT_SLOT)

   Value   0

   Min    0

   Max    4

  Event code 53 (ABS_MT_POSITION_X)

   Value   0

   Min    0

   Max   1023

  Event code 54 (ABS_MT_POSITION_Y)

   Value   0

   Min    0

   Max   599

  Event code 57 (ABS_MT_TRACKING_ID)

   Value   0

   Min    0

   Max  65535

Properties:

 Property type 1 (INPUT_PROP_DIRECT)

Testing ... (interrupt to exit)

Event: time 1659402314.202796, type 3 (EV_ABS), code 57 (ABS_MT_TRACKING_ID), value 6

Event: time 1659402314.202796, type 3 (EV_ABS), code 53 (ABS_MT_POSITION_X), value 348

Event: time 1659402314.202796, type 3 (EV_ABS), code 54 (ABS_MT_POSITION_Y), value 416

Event: time 1659402314.202796, type 1 (EV_KEY), code 330 (BTN_TOUCH), value 1

Event: time 1659402314.202796, type 3 (EV_ABS), code 0 (ABS_X), value 348

Event: time 1659402314.202796, type 3 (EV_ABS), code 1 (ABS_Y), value 416

Event: time 1659402314.202796, -------------- SYN_REPORT ------------

Event: time 1659402314.214664, type 3 (EV_ABS), code 53 (ABS_MT_POSITION_X), value 347

Event: time 1659402314.214664, type 3 (EV_ABS), code 0 (ABS_X), value 347

Event: time 1659402314.214664, -------------- SYN_REPORT ------------

Event: time 1659402314.296616, type 3 (EV_ABS), code 57 (ABS_MT_TRACKING_ID), value -1

Event: time 1659402314.296616, type 1 (EV_KEY), code 330 (BTN_TOUCH), value 0

Event: time 1659402314.296616, -------------- SYN_REPORT ------------

​

I can detect events, but the screen just doesn't respond.

Gregory PLANCHON
ST Technical Moderator
August 9, 2022

Hello,

I am looking for the cause of the problem and I need to know your use case to try to understand.

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
zxiao.4
zxiao.4AuthorBest answer
Associate III
August 11, 2022

I've fixed it. It should be the problem of touch coordinates. I just rotate in the device tree and reverse direction.