Status: errUNKNOWN, State: dfuERROR - What could this error be referring to?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-09 11:48 AM
I'm getting these errors on the consoles when FSBL (TF-A) is trying to download SSBL (U-Boot). What could this DFU error be? I've added the following to the U-Boot DTSI file so it ignore USB OTG VBUS and USB OTG ID. I've tried this using Linux and Windows with STProgrammer.
&usbotg_hs {
u-boot,force-b-session-valid;
dr_mode = "peripheral";
};
Console Output:
NOTICE: CPU: STM32MP157AAA Rev.Z
NOTICE: (a)Model: STMicroelectronics custom STM32CubeMX board - openstlinux-5.15-yocto-kirkstone-mp1-v22. 06.15
NOTICE: board_id = 0
NOTICE: Board: Board ID is zero
NOTICE: Checking fixed regulator register
INFO: fixed_regulator_register() is the problem
INFO: Entering the loop
INFO: register fixed reg regulator-vdd!
INFO: Node: 10728
NOTICE: Calling stm32mp1_syscfg_init()
WARNING: VDD unknown
NOTICE: Watchdog refresh
NOTICE: BSEC read debug configuration
NOTICE: Arch security setup
INFO: Reset reason (0x4):
INFO: Pad Reset from NRST
NOTICE: Syscfg enable IO
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
NOTICE: BL MEM param handling
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: Done with arch setup
NOTICE: BL2: v2.6-stm32mp1-r2.0(debug):()
NOTICE: BL2: Built : 17:01:00, Feb 8 2023
INFO: BL2: Doing platform setup
NOTICE: STM32MP DDR probe
INFO: RAM: DDR3-DDR3L 16bits 532000kHz
NOTICE: stm32mp_ddr_test_addr_bus(size) - size = 536870912
NOTICE: Checking for address bits stuck high
NOTICE: Checking for address bits stuck low
NOTICE: uret Value = 0
INFO: Memory size = 0x20000000 (512 MB)
INFO: DFU USB START LOAD...
INFO: DFU STATE - Phase=3, Address=c7000000, Base=c7000000, Length=16777216
STProgrammer Console Output
DFU State = 5
13:36:57:326 : Segment[0] downloaded successfully
13:36:57:326 : File download complete
13:36:57:326 : Time elapsed during download operation: 00:00:01.406
13:36:57:326 : RUNNING Program ...
13:36:57:326 : PartID: :0x01
13:36:57:326 : DFU status = 0
13:36:57:327 : DFU State = 5
13:36:57:327 : sending a dfu end of download request
13:36:57:328 : DFU status = 0
13:36:57:329 : DFU State = 7
13:36:57:476 : DFU status = 0
13:36:57:477 : DFU State = 2
13:36:57:477 : sending a set alternate setting request with index: 5
13:36:57:478 : receiving packet
13:36:57:479 : DFU status = 0
13:36:57:479 : DFU State = 2
13:36:57:479 : UpLoading data
13:36:57:482 : DFU status = 0
13:36:57:482 : DFU State = 2
13:36:57:482 : sending a set alternate setting request with index: 3
13:36:57:482 : Start operation done successfully at partition 0x01
13:36:57:482 : sending a set alternate setting request with index: 5
13:36:57:483 : receiving packet
13:36:57:483 : sending a clear status request
13:36:57:483 : an error occured after sending the clear status request
13:36:57:483 : Status: errUNKNOWN, State: dfuERROR
13:36:57:483 : sending a clear status request
13:36:57:483 : an error occured after sending the clear status request
13:36:57:483 : Status: errUNKNOWN, State: dfuERROR
13:36:57:483 : sending a clear status request
13:36:57:484 : an error occured after sending the clear status request
13:36:57:484 : Status: errUNKNOWN, State: dfuERROR
13:36:57:484 : sending a clear status request
13:36:57:487 : an error occured after sending the clear status request
13:36:57:487 : Status: errUNKNOWN, State: dfuERROR
13:36:57:487 : sending a clear status request
13:36:57:489 : DFU status = 14
13:36:57:489 : DFU State = 10
13:36:57:489 : an error occured after sending the clear status request
13:36:57:491 : Status: errUNKNOWN, State: dfuERROR
13:36:57:491 : sending a clear status request
13:36:57:491 : DFU status = 0
13:36:57:491 : DFU State = 2
13:36:57:491 : UpLoading data
13:36:57:507 : DFU status = 0
13:36:57:507 : DFU State = 2
13:36:57:507 : sending a set alternate setting request with index: 3
13:36:57:507 : Memory Programming ...
13:36:57:507 : Opening and parsing file: fip-stm32mp153a-xpro-mp1-mx-optee.bin
13:36:57:509 : File : fip-stm32mp153a-xpro-mp1-mx-optee.bin
13:36:57:511 : Size : 1.41 MB
13:36:57:511 : Partition ID : 0x03
13:36:57:511 : Download in Progress:
13:36:57:512 : Size : 1483254 Bytes
13:36:57:512 : sending packet nbr: 0
13:36:57:512 : Status: 14, State: 10
13:36:57:512 : sending a clear status request
13:36:57:513 : an error occured after sending the clear status request
13:36:57:513 : Status: errUNKNOWN, State: dfuERROR
13:36:57:513 : sending a clear status request
13:36:57:516 : an error occured after sending the clear status request
13:36:57:516 : Status: errUNKNOWN, State: dfuERROR
13:36:57:516 : sending a clear status request
13:36:57:516 : DFU status = 14
13:36:57:516 : DFU State = 10
13:36:57:516 : an error occured after sending the clear status request
13:36:57:516 : Status: errUNKNOWN, State: dfuERROR
13:36:57:517 : sending a clear status request
13:36:57:517 : DFU status = 0
13:36:57:518 : DFU State = 2
13:36:57:519 : DFU status = 0
13:36:57:519 : DFU State = 3
13:36:57:519 : DFU status = 0
13:36:57:519 : DFU State = 5
13:36:57:519 : sending packet nbr: 1
13:36:57:519 : DFU status = 0
13:36:57:519 : DFU State = 5
13:36:57:519 : Status: 0, State: 5
13:36:57:519 : DFU status = 0
13:36:57:519 : DFU State = 3
13:36:57:519 : Error during download get_status
13:36:57:519 : Error: failed to download Segment[0]
13:36:57:519 : Error: failed to download the File
13:36:57:538 : Error: Download partition 0x03 failed
13:36:57:560 : Error: TSV flashing service failed
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-09 12:24 PM
Is there not a version of this for TF-A? It almost seems like it's waiting for something to happen on the USB/DFU side but it never does. Eventually just times out. Custom target does not use USB OTG VBUS or USB OTG ID.
&usbotg_hs {
u-boot,force-b-session-valid;
dr_mode = "peripheral";
};
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-09 11:56 PM
Hi @Community member​
you need to add also:
usb-role-switch;
role-switch-default-mode = "peripheral";
Don't know if the various warning around VDD setting on your TF-A boot log might hurt.
Btw (maybe not the root cause of error), I see that your TF-A version (v2.6-stm32mp1-r2.0) is maybe not aligned with the Ecocsystem version (openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15)
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-10 6:37 AM
Hi Patrick,
Great catch! That's one Wiki page set I haven't run across. I'll give that a go in the TF-A DTS file.
As for the VDD warning, that's from my addition to get around my fixed power supply. I found nothing very concise on handling not using a PMIC but found example DTS's and parroted those. Here's how I've done that. Had other regulators listed as well but the compiler didn't like those so removed them.
regulators {
vdd: regulator-vdd {
compatible = "regulator-fixed";
regulator-name = "vdd";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
};
};
&pwr_regulators {
pwr-supply = <&vdd>;
};
That's weird my TF-A version isn't aligned with my Ecosystem. It should be, it all came together in 4.1.0 recently.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-10 8:11 AM
So I tried adding the following to the TF-A DTS
&usbotg_hs{
pinctrl-names = "default";
pinctrl-0 = <&usb_otg_hs_pins_mx>;
status = "okay";
/* USER CODE BEGIN usbotg_hs */
/*compatible = "st,stm32mp15-hsotg", "snps,dwc2"; /* 0: UTMI switch selects the OTG controller */
/*phys = <&usbphyc_port1 0>;
/*phy-names = "usb2-phy"; /* could be "host", see USB generic bindings */
dr_mode = "peripheral"; /* see USB generic bindings */
usb-role-switch; /* could be "host", see USB generic bindings */
role-switch-default-mode = "peripheral"; /* enable OTG */
/* USER CODE END usbotg_hs */
};
I tried with/without the compatibility and the phy entries. Same result. On the console TF-A is waiting on something to happen over USB it seems. I've added prints to the USB area in TF-A and it repeatedly tries to get started but never does. Sometimes it'll show on the programmer side stage 2 indicating it's going to download the optee bin file but never gets started. Seems to have gotten a little more difficult to track down in source code what's happening so a bit of a challenge to debug.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-10 8:40 AM
Did you check for classic pitfalls ?
https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-10 9:03 AM
Yeah, gone through that several times now.