2020-08-17 11:56 PM
Dear All,
According to AN5256 "discrete power supply hardware integration" the power source for VDD is turned off in case of crash to "reset" the hardware using the PWR_ONRST signal. At startup. At cold startup and immediately after a crash the power source for VDD has to be enabled. How the PWR_ONRST signal is drived on in this case as the MPU is not power at all ?
Thanks in advance for any help
2020-08-18 2:17 AM
Hi @PGE ,
The crash mentioned in AN5256 is caused by watchdog - "Crash (watchdog elapsed)". It means that MPU is normally powered at that moment and the crash is controlled by MPU to recover from e.g. endless loop. PWR_ONRST is genereted in inform outside world.
Hope this helps
Milan
2020-08-18 5:55 AM
Thanks for your reply!
Could you please confirm that VDD is always on and never ever interrupted even in case of crash recovery ?