cancel
Showing results for 
Search instead for 
Did you mean: 

Fail to reset from linux

fpoussin
Associate III

I'm having trouble resetting the board from linux.

Not using a PMIC but discrete power supplies.

I followed the app notes and errata, connecting the NRST and CORE_NRST pins with a cap then later a 0R resistor.

I'm using a single 100nF cap on NRST.

I can see the reset pin going down when rebooting from linux, unfortunately the MPU just freezes.

It looks like it gets stuck in BootROM after reset.

So far only a very long pull down (250ms+) on NRST works.

This or cycling power on VDDCORE which I can't do on my current prototype... (PWR_ON wired directly to VDDCORE supply enable pin)

Reset works fine from u-boot. (booting from SDMMC1, so already enabled)

I remember reset working a while ago, so I'll try to reproduce it and see what is blocking.

Any ideas?

NRST + CORE_NRST signals: (connected together)

0693W00000FDZNVQA5.png

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

I found the issue, it's caused by a circuit on my board: I use VBUS to control a transistor that pulls down some boot pins in order to upload firmware when plugged as a usb device.

There is a capacitor on VBUS that prevents this transistor to turn off fast enough until it reaches BootRom on reset.

View solution in original post

3 REPLIES 3
fpoussin
Associate III

Beginning of answer, reset works when I remove some of the regulators I use for peripherals from the DTS files.

These are simple "fixed-regulator" nodes that use a GPIO connected to a standard power switch ic.

Very strange issue... maybe current injection?

	reg_vbus: reg_vbus {
		compatible = "regulator-fixed";
		regulator-name = "vbus";
		regulator-min-microvolt = <5000000>;
		regulator-max-microvolt = <5000000>;
		vin-supply = <&vin>;
		gpio = <&gpiog 7 GPIO_ACTIVE_HIGH>;
		enable-active-high;
		regulator-always-on;
		startup-delay-us = <1000000>;
	};
 
	reg_canbus: reg_canbus {
		compatible = "regulator-fixed";
		regulator-name = "canbus";
		regulator-min-microvolt = <5000000>;
		regulator-max-microvolt = <5000000>;
		vin-supply = <&vin>;
		gpio = <&gpiob 10 GPIO_ACTIVE_HIGH>;
		enable-active-high;
		regulator-always-on;
	};

PatrickF
ST Employee

Hi,

NRST+NRST_CORE wired together should work fine if your platform is using VDD>2.7V (i.e. 3.0 or 3.3V typ.).

Did you ensure your boot Flash memory is correctly reset (or power-cycled) ?

As an example, SD-Card setup in UHS-I mode (i.e. I/O 1.8V) cannot go back to standard boot mode until a power cycle is applied.

If Boot is stuck in BootROM, please use https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_trace_analyzer and provide the traces.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I found the issue, it's caused by a circuit on my board: I use VBUS to control a transistor that pulls down some boot pins in order to upload firmware when plugged as a usb device.

There is a capacitor on VBUS that prevents this transistor to turn off fast enough until it reaches BootRom on reset.