Hi @Eldam .I've just tried running M4 code on "st-image-core" - on both ecosystems 1.2 and 2.0 following steps:https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/Linux_remoteproc_framework_overview#How_to_use_the_frameworkAnd everything works.Could yo...
Hello @浩 张 ,There's no such example for STM32MP1 but this audio codec is used on L4 discovery board, see:https://www.st.com/resource/en/user_manual/dm00353127-discovery-kit-with-stm32l496ag-mcu-stmicroelectronics.pdfYou can reuse the code from the a...
Hello @IBoak.1 ,To can use this tool to either flash sdcard or create image for dd command. https://hddguru.com/software/HDD-Raw-Copy-Tool/The other option is to follow instruction for yocto and use Cube programmer to flash it .Hope this helpsMilan
Hi @PBart.3 ,two concurrent debug sessions in one instance of CubeIDE are possible, see:https://community.st.com/s/question/0D50X0000Byue7DSQQ/regression-with-cubeide-v120-breakpoint-ignored-Some hints how to establish the debug sessions:https://com...