2022-02-02 7:21 PM
I've added OPENAMP through the middleware after enableing the IPCC interrupts, but now I'm getting the following error and an error in the actual OPENAMP source that's included!
/opt/st/stm32cubeide_1.8.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.linux64_2.0.0.202105311346/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld: ./Core/Src/main.o: in function `main':
/home/mschem/Gown-Sealer/STM32/sealer/CM4/Debug/../Core/Src/main.c:127: undefined reference to `MX_OPENAMP_Init'
/opt/st/stm32cubeide_1.8.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.linux64_2.0.0.202105311346/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld: /home/mschem/Gown-Sealer/STM32/sealer/CM4/Debug/../Core/Src/main.c:172: undefined reference to `OPENAMP_check_for_message'
/opt/st/stm32cubeide_1.8.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.linux64_2.0.0.202105311346/tools/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld: ./Middlewares/Third_Party/OpenAMP/virt_uart.o: in function `VIRT_UART_Init':
/home/mschem/Gown-Sealer/STM32/sealer/Middlewares/Third_Party/OpenAMP/virtual_driver/virt_uart.c:76: undefined reference to `OPENAMP_create_endpoint'
collect2: error: ld returned 1 exit status
make: *** [makefile:66: test_CM4.elf] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
2022-03-16 4:06 AM
Hi @msche.1 ,
Sorry to come late on this post.
I guess you find solution by yourself ?
Function OPENAMP_create_endpoint is declared in openamp.c/openamp.h
Olivier