cancel
Showing results for 
Search instead for 
Did you mean: 

i2c2

SergeyBlagodarnyy
Associate II

I'm working with the DevBoard from Myir MYD-YA-157C which has the stm32mp157 MPU. I'm trying to chech the i2c from the M4 in the Engineering mode and have a problem.

When I tied the I2C_TwoBoards_ComIT, it works. At least it generates the I2C5_ER_IRQ.

But when I move to the i2c2 or any other with pins that I have out, it doesn't work. Just doesn't do anything, doesn't send anyithng and doesn't generate an interrupt.

It is a simple test without any other peripherial enabled.

Could you help me what is wrong.

static void MX_I2C2_Init(void)
{
 
  hi2c2.Instance = I2C2;
  hi2c2.Init.Timing = 0x00701837;
  hi2c2.Init.OwnAddress1 = 783;
  hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_10BIT;
  hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
  hi2c2.Init.OwnAddress2 = 0;
  hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
  hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
  hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
  if (HAL_I2C_Init(&hi2c2) != HAL_OK)
  {
    Error_Handler();
  }
 
    /**Configure Analogue filter 
    */
  if (HAL_I2CEx_ConfigAnalogFilter(&hi2c2, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
  {
    Error_Handler();
  }
 
    /**Configure Digital filter 
    */
  if (HAL_I2CEx_ConfigDigitalFilter(&hi2c2, 0) != HAL_OK)
  {
    Error_Handler();
  }
 
  /**I2C Fast mode Plus enable
  */
  HAL_I2CEx_EnableFastModePlus(I2C_FASTMODEPLUS_I2C2);
}
 
void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)
{
 
  GPIO_InitTypeDef GPIO_InitStruct;
  if(hi2c->Instance==I2C2)
  {
  /* USER CODE BEGIN I2C2_MspInit 0 */
    if(IS_ENGINEERING_BOOT_MODE())
    {
      RCC_PeriphCLKInitTypeDef  RCC_PeriphCLKInitStruct;
  
      /*##-1- Configure the I2C clock source #*/
      RCC_PeriphCLKInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2C12;
      RCC_PeriphCLKInitStruct.I2c12ClockSelection = RCC_I2C12CLKSOURCE_HSI;
      HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphCLKInitStruct);
    }
  /* USER CODE END I2C2_MspInit 0 */
  
    /**I2C2 GPIO Configuration
    PZ6     ------> I2C2_SCL
    PZ7     ------> I2C2_SDA
    */
    GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF3_I2C2;
    PERIPH_LOCK(GPIOZ);
    HAL_GPIO_Init(GPIOZ, &GPIO_InitStruct);
    PERIPH_UNLOCK(GPIOZ);
    /* Peripheral clock enable */
    __HAL_RCC_I2C2_CLK_ENABLE();
    /* I2C2 interrupt Init */
    HAL_NVIC_SetPriority(I2C2_EV_IRQn, DEFAULT_IRQ_PRIO, 0);
    HAL_NVIC_EnableIRQ(I2C2_EV_IRQn);
    HAL_NVIC_SetPriority(I2C2_ER_IRQn, DEFAULT_IRQ_PRIO, 0);
    HAL_NVIC_EnableIRQ(I2C2_ER_IRQn);
  /* USER CODE BEGIN I2C2_MspInit 1 */
 
  /* USER CODE END I2C2_MspInit 1 */
  }
 
}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @SergeyBlagodarnyy​ ,

Sorry to come late on this post.

Did you find solution by yourself ?

Where do you stand ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.