2024-04-18 2:26 PM
I'm buildning my own computer by using STM32MP151AAC3.
I'm going to draw lines for the HDMI connector. I have one question: Can I transfer sound via the HDMI cable? For example if I run OpenSTLinux onto the STM32MP151AAC3 processor, and then I connect the HDMI cable and I can see the screen. Will I be able to hear sound too if I surf into Youtube?
Solved! Go to Solution.
2024-10-29 1:41 PM
Hi!
I solved the problem. Now I can hear sound from my SII9022A PHY.
I did not use ASoC Graph Card, instead I used Simple Card inside Linux kernel.
I post the Linux Device Tree in case if some one in the future want to play some music through the SII9022A.
// SPDX-License-Identifier: (GPL-2.0-or-later OR BSD-3-Clause)
/*
* Copyright (C) 2024, STMicroelectronics - All Rights Reserved
* Author: STM32CubeMX code generation for STMicroelectronics.
*/
/* For more information on Device Tree configuration, please refer to
* https://wiki.st.com/stm32mpu/wiki/Category:Device_tree_configuration
*/
/dts-v1/;
#include <dt-bindings/pinctrl/stm32-pinfunc.h>
#include "stm32mp151.dtsi"
#include "stm32mp15xa.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15-m4-srm.dtsi"
/* USER CODE BEGIN includes */
#include "stm32mp15-scmi.dtsi"
#include <dt-bindings/gpio/gpio.h>
#include <dt-bindings/mfd/st,stpmic1.h>
/* USER CODE END includes */
/ {
model = "STMicroelectronics custom STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mpu-v24.06.26";
compatible = "st,stm32mp151a-stm32-computer-firmware-mx", "st,stm32mp151";
memory@c0000000 {
device_type = "memory";
reg = <0xc0000000 0x20000000>;
/* USER CODE BEGIN memory */
/* USER CODE END memory */
};
reserved-memory {
#address-cells = <1>;
#size-cells = <1>;
ranges;
/* USER CODE BEGIN reserved-memory */
optee@de000000 {
reg = <0xde000000 0x2000000>;
no-map;
};
mcuram2:mcuram2@10000000{
compatible = "shared-dma-pool";
reg = <0x10000000 0x40000>;
no-map;
};
vdev0vring0:vdev0vring0@10040000{
compatible = "shared-dma-pool";
reg = <0x10040000 0x1000>;
no-map;
};
vdev0vring1:vdev0vring1@10041000{
compatible = "shared-dma-pool";
reg = <0x10041000 0x1000>;
no-map;
};
vdev0buffer:vdev0buffer@10042000{
compatible = "shared-dma-pool";
reg = <0x10042000 0x4000>;
no-map;
};
mcu_rsc_table:mcu-rsc-table@10048000{
compatible = "shared-dma-pool";
reg = <0x10048000 0x8000>;
no-map;
};
mcuram:mcuram@30000000{
compatible = "shared-dma-pool";
reg = <0x30000000 0x40000>;
no-map;
};
retram:retram@38000000{
compatible = "shared-dma-pool";
reg = <0x38000000 0x10000>;
no-map;
};
/* USER CODE END reserved-memory */
};
/* USER CODE BEGIN root */
aliases{
ethernet0 = ðernet0;
serial0 = &uart4;
};
hdmi:connector{
compatible = "hdmi-connector";
#sound-dai-cells = <0>;
label = "hdmi";
type = "a";
port{
hdmi_connector_in:endpoint{
remote-endpoint = <&sii9022_out>;
};
hdmi_audio_out:endpoit{
remote-endpoint= <&sii9022_tx_endpoint>;
};
};
};
sound {
compatible = "simple-audio-card";
simple-audio-card,name = "SII9022A HDMI";
simple-audio-card,format = "i2s";
/*simple-audio-card,widgets = "Speaker", "External Speaker";
simple-audio-card,routing = "External Speaker", "LINE_OUT";*/
simple-audio-card,bitclock-master = <&dailink0_master>;
simple-audio-card,frame-master = <&dailink0_master>;
simple-audio-card,mclk-fs = <256>;
dailink0_master: simple-audio-card,cpu {
sound-dai = <&i2s2>;
};
simple-audio-card,codec {
sound-dai = <&sii9022A>;
};
};
config {
u-boot,boot-led = "heartbeat";
u-boot,error-led = "error";
u-boot,mmc-env-partition = "u-boot-env";
st,fastboot-gpios = <&gpioa 13 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
st,stm32prog-gpios = <&gpioa 14 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
};
led{
compatible = "gpio-leds";
led-blue{
label = "heartbeat";
gpios = <&gpioa 14 GPIO_ACTIVE_LOW>;
linux,default-trigger = "timer"; /* Change from heartbeat -> timer */
default-state = "off";
};
led-red {
label = "error";
gpios = <&gpioa 13 GPIO_ACTIVE_LOW>;
default-state = "off";
};
};
vin:vin{
compatible = "regulator-fixed";
regulator-name = "vin";
regulator-min-microvolt = <5000000>;
regulator-max-microvolt = <5000000>;
regulator-always-on;
};
chosen{
stdout-path = "serial0:115200n8";
};
/* USER CODE END root */
clocks{
/* USER CODE BEGIN clocks */
clk_csi: clk-csi {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <4000000>;
};
clk_hse: clk-hse {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <24000000>;
};
clk_hsi: clk-hsi {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <64000000>;
};
clk_lse: clk-lse {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <32768>;
};
clk_lsi: clk-lsi {
#clock-cells = <0>;
compatible = "fixed-clock";
clock-frequency = <32000>;
};
/* USER CODE END clocks */
};
}; /*root*/
&pinctrl {
eth1_pins_mx: eth1_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 1, AF11)>, /* ETH1_RX_CLK */
<STM32_PINMUX('A', 7, AF11)>, /* ETH1_RX_CTL */
<STM32_PINMUX('B', 0, AF11)>, /* ETH1_RXD2 */
<STM32_PINMUX('C', 4, AF11)>, /* ETH1_RXD0 */
<STM32_PINMUX('C', 5, AF11)>, /* ETH1_RXD1 */
<STM32_PINMUX('H', 7, AF11)>; /* ETH1_RXD3 */
bias-disable;
};
pins2 {
pinmux = <STM32_PINMUX('A', 2, AF11)>; /* ETH1_MDIO */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
pins3 {
pinmux = <STM32_PINMUX('B', 11, AF11)>, /* ETH1_TX_CTL */
<STM32_PINMUX('C', 1, AF11)>, /* ETH1_MDC */
<STM32_PINMUX('C', 2, AF11)>, /* ETH1_TXD2 */
<STM32_PINMUX('E', 2, AF11)>, /* ETH1_TXD3 */
<STM32_PINMUX('G', 4, AF11)>, /* ETH1_GTX_CLK */
<STM32_PINMUX('G', 5, AF11)>, /* ETH1_CLK125 */
<STM32_PINMUX('G', 13, AF11)>, /* ETH1_TXD0 */
<STM32_PINMUX('G', 14, AF11)>; /* ETH1_TXD1 */
bias-disable;
drive-push-pull;
slew-rate = <2>;
};
pins4 {
pinmux = <STM32_PINMUX('B', 5, AF0)>; /* ETH1_CLK */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
};
eth1_sleep_pins_mx: eth1_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 1, ANALOG)>, /* ETH1_RX_CLK */
<STM32_PINMUX('A', 2, ANALOG)>, /* ETH1_MDIO */
<STM32_PINMUX('A', 7, ANALOG)>, /* ETH1_RX_CTL */
<STM32_PINMUX('B', 0, ANALOG)>, /* ETH1_RXD2 */
<STM32_PINMUX('B', 5, ANALOG)>, /* ETH1_CLK */
<STM32_PINMUX('B', 11, ANALOG)>, /* ETH1_TX_CTL */
<STM32_PINMUX('C', 1, ANALOG)>, /* ETH1_MDC */
<STM32_PINMUX('C', 2, ANALOG)>, /* ETH1_TXD2 */
<STM32_PINMUX('C', 4, ANALOG)>, /* ETH1_RXD0 */
<STM32_PINMUX('C', 5, ANALOG)>, /* ETH1_RXD1 */
<STM32_PINMUX('E', 2, ANALOG)>, /* ETH1_TXD3 */
<STM32_PINMUX('G', 4, ANALOG)>, /* ETH1_GTX_CLK */
<STM32_PINMUX('G', 5, ANALOG)>, /* ETH1_CLK125 */
<STM32_PINMUX('G', 13, ANALOG)>, /* ETH1_TXD0 */
<STM32_PINMUX('G', 14, ANALOG)>, /* ETH1_TXD1 */
<STM32_PINMUX('H', 7, ANALOG)>; /* ETH1_RXD3 */
};
};
hdmi_cec_pins_mx: hdmi_cec_mx-0 {
pins {
pinmux = <STM32_PINMUX('B', 6, AF5)>; /* CEC */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
hdmi_cec_sleep_pins_mx: hdmi_cec_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('B', 6, ANALOG)>; /* CEC */
};
};
i2c1_pins_mx: i2c1_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 12, AF5)>, /* I2C1_SCL */
<STM32_PINMUX('D', 13, AF5)>; /* I2C1_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
i2c1_sleep_pins_mx: i2c1_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 12, ANALOG)>, /* I2C1_SCL */
<STM32_PINMUX('D', 13, ANALOG)>; /* I2C1_SDA */
};
};
i2c4_pins_mx: i2c4_mx-0 {
pins {
pinmux = <STM32_PINMUX('F', 14, AF4)>, /* I2C4_SCL */
<STM32_PINMUX('F', 15, AF4)>; /* I2C4_SDA */
bias-disable;
drive-open-drain;
slew-rate = <0>;
};
};
i2c4_sleep_pins_mx: i2c4_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('F', 14, ANALOG)>, /* I2C4_SCL */
<STM32_PINMUX('F', 15, ANALOG)>; /* I2C4_SDA */
};
};
i2s2_pins_mx: i2s2_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 9, AF5)>, /* I2S2_CK */
<STM32_PINMUX('B', 12, AF5)>, /* I2S2_WS */
<STM32_PINMUX('I', 3, AF5)>; /* I2S2_SDO */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
};
i2s2_sleep_pins_mx: i2s2_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 9, ANALOG)>, /* I2S2_CK */
<STM32_PINMUX('B', 12, ANALOG)>, /* I2S2_WS */
<STM32_PINMUX('I', 3, ANALOG)>; /* I2S2_SDO */
};
};
ltdc_pins_mx: ltdc_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 3, AF14)>, /* LTDC_B5 */
<STM32_PINMUX('B', 1, AF14)>, /* LTDC_G0 */
<STM32_PINMUX('B', 8, AF14)>, /* LTDC_B6 */
<STM32_PINMUX('C', 0, AF14)>, /* LTDC_R5 */
<STM32_PINMUX('D', 8, AF14)>, /* LTDC_B7 */
<STM32_PINMUX('D', 9, AF14)>, /* LTDC_B0 */
<STM32_PINMUX('D', 10, AF14)>, /* LTDC_B3 */
<STM32_PINMUX('E', 6, AF14)>, /* LTDC_G1 */
<STM32_PINMUX('E', 15, AF14)>, /* LTDC_R7 */
<STM32_PINMUX('F', 10, AF14)>, /* LTDC_DE */
<STM32_PINMUX('G', 10, AF14)>, /* LTDC_B2 */
<STM32_PINMUX('G', 12, AF14)>, /* LTDC_B1 */
<STM32_PINMUX('H', 2, AF14)>, /* LTDC_R0 */
<STM32_PINMUX('H', 3, AF14)>, /* LTDC_R1 */
<STM32_PINMUX('H', 8, AF14)>, /* LTDC_R2 */
<STM32_PINMUX('H', 9, AF14)>, /* LTDC_R3 */
<STM32_PINMUX('H', 10, AF14)>, /* LTDC_R4 */
<STM32_PINMUX('H', 12, AF14)>, /* LTDC_R6 */
<STM32_PINMUX('H', 13, AF14)>, /* LTDC_G2 */
<STM32_PINMUX('H', 14, AF14)>, /* LTDC_G3 */
<STM32_PINMUX('H', 15, AF14)>, /* LTDC_G4 */
<STM32_PINMUX('I', 0, AF14)>, /* LTDC_G5 */
<STM32_PINMUX('I', 1, AF14)>, /* LTDC_G6 */
<STM32_PINMUX('I', 2, AF14)>, /* LTDC_G7 */
<STM32_PINMUX('I', 4, AF14)>, /* LTDC_B4 */
<STM32_PINMUX('I', 9, AF14)>, /* LTDC_VSYNC */
<STM32_PINMUX('I', 10, AF14)>; /* LTDC_HSYNC */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
pins2 {
pinmux = <STM32_PINMUX('G', 7, AF14)>; /* LTDC_CLK */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
};
ltdc_sleep_pins_mx: ltdc_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 3, ANALOG)>, /* LTDC_B5 */
<STM32_PINMUX('B', 1, ANALOG)>, /* LTDC_G0 */
<STM32_PINMUX('B', 8, ANALOG)>, /* LTDC_B6 */
<STM32_PINMUX('C', 0, ANALOG)>, /* LTDC_R5 */
<STM32_PINMUX('D', 8, ANALOG)>, /* LTDC_B7 */
<STM32_PINMUX('D', 9, ANALOG)>, /* LTDC_B0 */
<STM32_PINMUX('D', 10, ANALOG)>, /* LTDC_B3 */
<STM32_PINMUX('E', 6, ANALOG)>, /* LTDC_G1 */
<STM32_PINMUX('E', 15, ANALOG)>, /* LTDC_R7 */
<STM32_PINMUX('F', 10, ANALOG)>, /* LTDC_DE */
<STM32_PINMUX('G', 7, ANALOG)>, /* LTDC_CLK */
<STM32_PINMUX('G', 10, ANALOG)>, /* LTDC_B2 */
<STM32_PINMUX('G', 12, ANALOG)>, /* LTDC_B1 */
<STM32_PINMUX('H', 2, ANALOG)>, /* LTDC_R0 */
<STM32_PINMUX('H', 3, ANALOG)>, /* LTDC_R1 */
<STM32_PINMUX('H', 8, ANALOG)>, /* LTDC_R2 */
<STM32_PINMUX('H', 9, ANALOG)>, /* LTDC_R3 */
<STM32_PINMUX('H', 10, ANALOG)>, /* LTDC_R4 */
<STM32_PINMUX('H', 12, ANALOG)>, /* LTDC_R6 */
<STM32_PINMUX('H', 13, ANALOG)>, /* LTDC_G2 */
<STM32_PINMUX('H', 14, ANALOG)>, /* LTDC_G3 */
<STM32_PINMUX('H', 15, ANALOG)>, /* LTDC_G4 */
<STM32_PINMUX('I', 0, ANALOG)>, /* LTDC_G5 */
<STM32_PINMUX('I', 1, ANALOG)>, /* LTDC_G6 */
<STM32_PINMUX('I', 2, ANALOG)>, /* LTDC_G7 */
<STM32_PINMUX('I', 4, ANALOG)>, /* LTDC_B4 */
<STM32_PINMUX('I', 9, ANALOG)>, /* LTDC_VSYNC */
<STM32_PINMUX('I', 10, ANALOG)>; /* LTDC_HSYNC */
};
};
sdmmc2_pins_mx: sdmmc2_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
<STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('E', 3, AF9)>, /* SDMMC2_CK */
<STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-pull-up;
drive-push-pull;
slew-rate = <1>;
};
};
sdmmc2_opendrain_pins_mx: sdmmc2_opendrain_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('A', 8, AF9)>, /* SDMMC2_D4 */
<STM32_PINMUX('B', 3, AF9)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, AF9)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 9, AF10)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 15, AF9)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, AF10)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 5, AF9)>; /* SDMMC2_D6 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('B', 14, AF9)>, /* SDMMC2_D0 */
<STM32_PINMUX('E', 3, AF9)>; /* SDMMC2_CK */
bias-pull-up;
drive-push-pull;
slew-rate = <1>;
};
pins3 {
pinmux = <STM32_PINMUX('G', 6, AF10)>; /* SDMMC2_CMD */
bias-pull-up;
drive-open-drain;
slew-rate = <1>;
};
};
sdmmc2_sleep_pins_mx: sdmmc2_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 8, ANALOG)>, /* SDMMC2_D4 */
<STM32_PINMUX('B', 3, ANALOG)>, /* SDMMC2_D2 */
<STM32_PINMUX('B', 4, ANALOG)>, /* SDMMC2_D3 */
<STM32_PINMUX('B', 9, ANALOG)>, /* SDMMC2_D5 */
<STM32_PINMUX('B', 14, ANALOG)>, /* SDMMC2_D0 */
<STM32_PINMUX('B', 15, ANALOG)>, /* SDMMC2_D1 */
<STM32_PINMUX('C', 7, ANALOG)>, /* SDMMC2_D7 */
<STM32_PINMUX('E', 3, ANALOG)>, /* SDMMC2_CK */
<STM32_PINMUX('E', 5, ANALOG)>, /* SDMMC2_D6 */
<STM32_PINMUX('G', 6, ANALOG)>; /* SDMMC2_CMD */
};
};
uart4_pins_mx: uart4_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
bias-pull-up;
};
pins2 {
pinmux = <STM32_PINMUX('G', 11, AF6)>; /* UART4_TX */
bias-pull-up;
drive-push-pull;
slew-rate = <0>;
};
};
uart4_idle_pins_mx: uart4_idle_mx-0 {
pins1 {
pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */
bias-pull-up;
};
pins2 {
pinmux = <STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
bias-pull-up;
};
};
uart4_sleep_pins_mx: uart4_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('B', 2, ANALOG)>, /* UART4_RX */
<STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */
bias-pull-up;
};
};
usb_otg_hs_pins_mx: usb_otg_hs_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
};
};
usb_otg_hs_sleep_pins_mx: usb_otg_hs_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('A', 10, ANALOG)>; /* USB_OTG_HS_ID */
};
};
/* USER CODE BEGIN pinctrl */
/* USER CODE END pinctrl */
};
&pinctrl_z {
/* USER CODE BEGIN pinctrl_z */
/* USER CODE END pinctrl_z */
};
&m4_rproc{
status = "disabled";
/* USER CODE BEGIN m4_rproc */
resets = <&scmi_reset RST_SCMI_MCU>, <&scmi_reset RST_SCMI_MCU_HOLD_BOOT>;
reset-names = "mcu_rst", "hold_boot";
/*/delete-property/ st,syscfg-holdboot;*/
mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>, <&ipcc 3>;
mbox-names = "vq0", "vq1", "shutdown", "detach";
memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>, <&vdev0vring1>, <&vdev0buffer>, <&mcu_rsc_table>;
interrupt-parent = <&exti>;
interrupts = <68 1>;
wakeup-source;
/* USER CODE END m4_rproc */
m4_system_resources{
status = "disabled";
/* USER CODE BEGIN m4_system_resources */
/* USER CODE END m4_system_resources */
};
};
&bsec{
status = "okay";
/* USER CODE BEGIN bsec */
/* USER CODE END bsec */
};
&cec{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&hdmi_cec_pins_mx>;
pinctrl-1 = <&hdmi_cec_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN cec */
/* USER CODE END cec */
};
&dma1{
status = "okay";
/* USER CODE BEGIN dma1 */
resets = <&scmi_reset RST_SCMI_MDMA>;
/* USER CODE END dma1 */
};
&dma2{
status = "disabled";
/* USER CODE BEGIN dma2 */
/* USER CODE END dma2 */
};
&dmamux1{
status = "okay";
dma-masters = <&dma1>;
dma-channels = <8>;
/* USER CODE BEGIN dmamux1 */
/* USER CODE END dmamux1 */
};
ðernet0{
pinctrl-names = "default", "sleep";
pinctrl-0 = <ð1_pins_mx>;
pinctrl-1 = <ð1_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ethernet0 */
phy-mode = "rgmii-id";
max-speed = <1000>;
phy-handle = <&phy0>;
nvmem-cells = <ðernet_mac_address>;
nvmem-cell-names = "mac-address";
mdio{
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0:ethernet-phy@0{
reg = <0>;
};
};
/* USER CODE END ethernet0 */
};
&hsem{
status = "okay";
/* USER CODE BEGIN hsem */
/* USER CODE END hsem */
};
&i2c1{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c1_pins_mx>;
pinctrl-1 = <&i2c1_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2c1 */
/* USER CODE END i2c1 */
};
&i2c4{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c4_pins_mx>;
pinctrl-1 = <&i2c4_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2c4 */
clocks = <&scmi_clk CK_SCMI_I2C4>;
resets = <&scmi_reset RST_SCMI_I2C4>;
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <400000>;
/delete-property/ dmas;
/delete-property/ dma-names;
sii9022A: hdmi-transmitter@39{
compatible = "sil,sii9022";
reg = <0x39>;
iovcc-supply = <&v3v3_hdmi>;
cvcc12-supply = <&v1v2_hdmi>;
reset-gpios = <&gpioe 8 GPIO_ACTIVE_LOW>;
interrupts = <1 IRQ_TYPE_EDGE_FALLING>;
interrupt-parent = <&gpiog>;
#sound-dai-cells = <0>;
sil,i2s-data-lanes = <0>;
/*clocks = <&mclk>;
clock-names = "mclk";*/
status = "okay";
ports{
#address-cells = <1>;
#size-cells = <0>;
port@0{
reg = <0>;
sii9022_in:endpoint{
remote-endpoint = <<dc_ep0_out>;
};
};
port@1{
reg = <1>;
sii9022_out:endpoint{
remote-endpoint = <&hdmi_connector_in>;
};
};
port@3{
reg = <3>;
sii9022_tx_endpoint:endpoint{
remote-endpoint = <&i2s2_endpoint>;
};
};
};
};
pmic:stpmic@33{
compatible = "st,stpmic1";
reg = <0x33>;
/*interrupts-extended = <&gpioa 0 IRQ_TYPE_EDGE_FALLING>;*/
interrupts-extended = <&exti 55 IRQ_TYPE_EDGE_FALLING>;
interrupt-controller;
#interrupt-cells = <2>;
status = "okay";
regulators{
compatible = "st,stpmic1-regulators";
buck1-supply = <&vin>;
buck2-supply = <&vin>;
buck3-supply = <&vin>;
buck4-supply = <&vin>;
/*ldo1-supply = <&v3v3>;*/
ldo2-supply = <&vin>;
ldo3-supply = <&vdd_ddr>;
ldo4-supply = <&vin>;
ldo5-supply = <&vin>;
ldo6-supply = <&v3v3>;
vref_ddr-supply = <&vin>;
/*boost-supply = <&vin>;
pwr_sw1-supply = <&bst_out>;
pwr_sw2-supply = <&bst_out>;*/
vddcore:buck1{
regulator-name = "vddcore";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
vdd_ddr:buck2{
regulator-name = "vdd_ddr";
regulator-min-microvolt = <1350000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
vdd:buck3{
regulator-name = "vdd";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
st,mask-reset;
regulator-initial-mode = <0>;
regulator-over-current-protection;
};
v3v3:buck4{
regulator-name = "v3v3";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
regulator-over-current-protection;
regulator-initial-mode = <0>;
};
/*
v1v8_audio:ldo1{
regulator-name = "v1v8_audio";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
regulator-always-on;
interrupts = <IT_CURLIM_LDO1 0>;
};*/
v3v3_hdmi:ldo2{
regulator-name = "v3v3_hdmi";
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
regulator-always-on;
interrupts = <IT_CURLIM_LDO2 0>;
};
vtt_ddr:ldo3{
regulator-name = "vtt_ddr";
regulator-min-microvolt = <500000>;
regulator-max-microvolt = <750000>;
regulator-always-on;
regulator-over-current-protection;
};
vdd_usb:ldo4{
regulator-name = "vdd_usb";
interrupts = <IT_CURLIM_LDO4 0>;
};
vdda:ldo5{
regulator-name = "vdda";
regulator-min-microvolt = <2900000>;
regulator-max-microvolt = <2900000>;
interrupts = <IT_CURLIM_LDO5 0>;
regulator-boot-on;
};
v1v2_hdmi:ldo6{
regulator-name = "v1v2_hdmi";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1200000>;
regulator-always-on;
interrupts = <IT_CURLIM_LDO6 0>;
};
vref_ddr:vref-ddr{
regulator-name = "vref_ddr";
regulator-always-on;
};
/*
bst_out:boost{
regulator-name = "bst_out";
interrupts = <IT_OCP_BOOST 0>;
};
vbus_otg:pwr-sw1{
regulator-name = "vbus_otg";
interrupts = <IT_OCP_OTG 0>;
};
vbus_sw:pwr-sw2{
regulator-name = "vbus_sw";
interrupts = <IT_OCP_SWOUT 0>;
regulator-active-discharge = <1>;
};
*/
};
onkey{
compatible = "st,stpmic1-onkey";
interrupts = <IT_PONKEY_F 0>, <IT_PONKEY_R 0>;
interrupt-names = "onkey-falling", "onkey-rising";
power-off-time-sec = <10>;
status = "okay";
};
};
/* USER CODE END i2c4 */
};
&i2s2{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2s2_pins_mx>;
pinctrl-1 = <&i2s2_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2s2 */
clocks = <&rcc SPI2>, <&rcc SPI2_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "i2sclk", "x8k", "x11k";
i2s2_port:port{
i2s2_endpoint:endpoint{
remote-endpoint = <&sii9022_tx_endpoint>;
dai-format = "i2s";
mclk-fs = <256>;
};
};
/* USER CODE END i2s2 */
};
<dc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <<dc_pins_mx>;
pinctrl-1 = <<dc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN ltdc */
port{
ltdc_ep0_out:endpoint{
remote-endpoint = <&sii9022_in>;
};
};
/* USER CODE END ltdc */
};
&m4_dma2{
status = "okay";
/* USER CODE BEGIN m4_dma2 */
/* USER CODE END m4_dma2 */
};
&mdma1{
status = "okay";
/* USER CODE BEGIN mdma1 */
/* USER CODE END mdma1 */
};
&pwr_regulators{
status = "okay";
/* USER CODE BEGIN pwr_regulators */
vdd-supply = <&vdd>;
vdd_3v3_usbfs-supply = <&vdd_usb>;
/* USER CODE END pwr_regulators */
};
&rcc{
status = "okay";
/* USER CODE BEGIN rcc */
compatible = "st,stm32mp1-rcc-secure", "syscon";
clock-names = "hse", "hsi", "csi", "lse", "lsi";
clocks = <&scmi_clk CK_SCMI_HSE>,
<&scmi_clk CK_SCMI_HSI>,
<&scmi_clk CK_SCMI_CSI>,
<&scmi_clk CK_SCMI_LSE>,
<&scmi_clk CK_SCMI_LSI>;
/* USER CODE END rcc */
};
&rng1{
status = "okay";
/* USER CODE BEGIN rng1 */
clocks = <&scmi_clk CK_SCMI_RNG1>;
resets = <&scmi_reset RST_SCMI_RNG1>;
/* USER CODE END rng1 */
};
&rtc{
status = "okay";
/* USER CODE BEGIN rtc */
clocks = <&scmi_clk CK_SCMI_RTCAPB>, <&scmi_clk CK_SCMI_RTC>;
/* USER CODE END rtc */
};
&sdmmc2{
pinctrl-names = "default", "opendrain", "sleep";
pinctrl-0 = <&sdmmc2_pins_mx>;
pinctrl-1 = <&sdmmc2_opendrain_pins_mx>;
pinctrl-2 = <&sdmmc2_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN sdmmc2 */
non-removable;
no-sd;
no-sdio;
st,neg-edge;
bus-width = <8>;
vmmc-supply = <&v3v3>;
vqmmc-supply = <&vdd>;
mmc-ddr-3_3v;
/* USER CODE END sdmmc2 */
};
&tamp{
status = "okay";
/* USER CODE BEGIN tamp */
/* USER CODE END tamp */
};
&uart4{
pinctrl-names = "default", "idle", "sleep";
pinctrl-0 = <&uart4_pins_mx>;
pinctrl-1 = <&uart4_idle_pins_mx>;
pinctrl-2 = <&uart4_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN uart4 */
/delete-property/ dmas;
/delete-property/ dma-names;
u-boot,dm-pre-reloc;
/* USER CODE END uart4 */
};
&usbh_ehci{
status = "okay";
/* USER CODE BEGIN usbh_ehci */
phys = <&usbphyc_port0>;
#address-cells = <1>;
#size-cells = <0>;
/* onboard HUB */
hub@1 {
compatible = "usb424,2514";
reg = <1>;
vdd-supply = <&v3v3>;
};
/* USER CODE END usbh_ehci */
};
&usbh_ohci{
status = "okay";
/* USER CODE BEGIN usbh_ohci */
/* USER CODE END usbh_ohci */
};
&usbotg_hs{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&usb_otg_hs_pins_mx>;
pinctrl-1 = <&usb_otg_hs_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN usbotg_hs */
phys = <&usbphyc_port1 0>;
phy-names = "usb2-phy";
usb-role-switch;
u-boot,dm-pre-reloc;
u-boot,force-b-session-valid;
hnp-srp-disable;
dr_mode = "peripheral";
/* USER CODE END usbotg_hs */
};
&usbphyc{
status = "okay";
/* USER CODE BEGIN usbphyc */
phy-supply = <&vdd_usb>;
/* USER CODE END usbphyc */
};
&usbphyc_port0{
status = "okay";
/* USER CODE BEGIN usbphyc_port0 */
phy-supply = <&vdd_usb>;
st,tune-hs-dc-level = <2>;
st,enable-fs-rftime-tuning;
st,enable-hs-rftime-reduction;
st,trim-hs-current = <15>;
st,trim-hs-impedance = <1>;
st,tune-squelch-level = <3>;
st,tune-hs-rx-offset = <2>;
st,no-lsfs-sc;
/* USER CODE END usbphyc_port0 */
};
&usbphyc_port1{
status = "okay";
/* USER CODE BEGIN usbphyc_port1 */
phy-supply = <&vdd_usb>;
st,tune-hs-dc-level = <2>;
st,enable-fs-rftime-tuning;
st,enable-hs-rftime-reduction;
st,trim-hs-current = <15>;
st,trim-hs-impedance = <1>;
st,tune-squelch-level = <3>;
st,tune-hs-rx-offset = <2>;
st,no-lsfs-sc;
/* USER CODE END usbphyc_port1 */
};
/* USER CODE BEGIN addons */
/*
&arm_wdt{
timeout-sec = <32>;
status = "okay";
};
*/
&cpu0 {
cpu-supply = <&vddcore>;
clocks = <&scmi_clk CK_SCMI_MPU>;
};
&uart4_pins_mx {
u-boot,dm-pre-reloc;
pins1 {
u-boot,dm-pre-reloc;
};
pins2 {
u-boot,dm-pre-reloc;
};
};
&gpioz {
clocks = <&scmi_clk CK_SCMI_GPIOZ>;
};
/* USER CODE END addons */
2024-04-19 7:54 AM
Hi @DMårt
note that performance of STM32MP151A as general purpose 'computer' might be deceptive. I think you could forget Youtube video thru HTML browsing (e.g. no high-resolution capable and only SW video decoder).
Anyway, no issue to output audio on HDMI, please refer to STM32MP157F-DK2 reference design.
Regards.
2024-04-20 5:48 AM
Thank you for your reply.
I have no plats to have that STM32MP151AAC3 as a general purpose computer. But I have plans to have a GUI application onto it, written in C or C++ or Java.
Is that possible? 3D or 2D.
2024-04-22 12:04 AM
Hi,
no issue to have nice GUI with STM32MP151.
3D is possible, but without GPU and with single-core Cortex-A7, might not be best performances.
Regards.
2024-10-20 4:02 PM
Hi!
Is there any software In need? Like Alsa Mixer?
I assuming that In need to read the data fram I2S2.
2024-10-20 11:34 PM
Hi,
audio on HDMI is available on STM32MP157F-DK2.
You should use I2S (from SAI or SPI having I2S).
For SW, I think you need ALSA plus some drivers for the HDMI chipset, but I'm not expert.
https://wiki.st.com/stm32mpu/wiki/ALSA_overview
Regards
2024-10-22 3:16 PM - edited 2024-10-22 3:27 PM
Hi! @PatrickF
Thank you for your reply. I have enabled I2S and my Linux system can now see the i2s device when I write
dmesg | grep i2s
According to this URL: https://wiki.st.com/stm32mpu/wiki/I2S_Linux_driver
It says:
The I2S Linux driver can be accessed from userland through an ALSA device.
Refer to ALSA overview for information on how to list and use ALSA devices.
So I head over to the ALSA overview. https://wiki.st.com/stm32mpu/wiki/ALSA_overview
It says:
The ALSA/ASoC and the audio graph card must be enabled in the kernel configuration, as shown below, to enable the sound support.
On top of this, the user has to activate the CPU and Codec drivers according to the chosen hardware.
The user can use Linux Menuconfig tool to select the required drivers:
And that is refering to enable:
[*] Device Drivers
[*] Sound card support
[*] Advanced Linux Sound Architecture
[*] ALSA for SoC audio support
STMicroelectronics STM32 SOC audio support
[ ] STM32 SAI interface (Serial Audio Interface) support
[ ] STM32 I2S interface (SPI/I2S block) support
[ ] STM32 S/PDIF receiver (SPDIFRX) support
CODEC drivers
[ ] ...
[*] ASoC Audio Graph sound card support <--- This one
But does this mean that the ASoC Audio Graph sound card support is another card and not i2s?
Because in the Dev-board of STM32MP1 series. They contains a special old-school (imo) audio jack and a chip that are connected to i2s. Is this the "sound card" the wiki refering to? It's from STM32MP15-DISCO board.
My situation:
In my situation, I want to use the I2S bus which linux is recognizing, together with SII9022A HDMI PHY.
This question is more like a software-recommendation question, rather than a programming/configuration question.
I have installed alsa-utils and wrote
aplay -l
. This gave me the information that there are no sound cards found. But I'm not looking for a sound card. Only a way to transfer sound to SII9022A, which is my "sound card", if we are going to use the same terms as linux is using.
If ST have no support nor answer for enable music through i2s to SII9022A, please let me know. Then I will look somewhere else.
2024-10-22 11:25 PM
Hi,
Did you have a look to Device Tree of STM32MP157F-DK2 (search for '9022')?
https://github.com/STMicroelectronics/linux/blob/v6.1-stm32mp/arch/arm/boot/dts/stm32mp15xx-dkx.dtsi
This board use Sii9022 HDMI with Audio thru i2S2.
root@stm32mp1:~# alsactl info
#
# Sound card
#
- card: 0
id: STM32MP15DK
name: STM32MP15-DK
longname: STM32MP15-DK
driver_name: STM32MP15-DK
mixer_name:
components:
controls_count: 23
pcm:
- stream: PLAYBACK
devices:
- device: 0
id: 4400b004.audio-controller-cs42l51-hifi cs42l51-hifi-0
name: 4400b004.audio-controller-cs42l51-hifi cs42l51-hifi-0
subdevices:
- subdevice: 0
name: subdevice #0
- device: 2
id: 4000b000.audio-controller-i2s-hifi i2s-hifi-2
name: 4000b000.audio-controller-i2s-hifi i2s-hifi-2
subdevices:
- subdevice: 0
name: subdevice #0
From RefMan, 4000b000 correspond to SPI2/I2S2
Hope it's help.
Regards.
2024-10-23 1:46 AM
I think I must find a way to enable ASoC Graph Card inside the Linux kernel. I was not sure if ASoC was for SII9022A or not. I will try that and give you a reply later.
Thank you.
By the way! Every time i change the .config file and try to compile, then the output says that I need to run "make mrproper" inside the source folder of Linux. So I just copy the .config to the build folder of Linux.
One question more: When can I buy STM32MP2 series? The distributors seems been out of stock.
2024-10-23 3:18 AM - edited 2024-10-23 3:29 AM
Hi again!
I activated [*] the ASoC Audio Graph sound card support together with STM32 I2S interface (SPI/I2S block) support .
I can see the 4000b000.audio-controller when I write dmesg | grep i2s.
I cannot se any soundcard when I write aplay -l or alsactl info. Is there any step I have missed such as activate alsa or i2s as a unit?
Do you see any potential errors in my device tree? I don't have SAI enabled.
hdmi:connector{
compatible = "hdmi-connector";
label = "hdmi";
type = "a";
port{
hdmi_connector_in:endpoint{
remote-endpoint = <&sii9022_out>;
};
};
};
sound {
compatible = "audio-graph-card";
label = "STM32MP15-DK";
routing =
"Playback" , "MCLK",
"Capture" , "MCLK",
"MICL" , "Mic Bias";
dais = <&i2s2_port>;
status = "okay";
};
&i2s2{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2s2_pins_mx>;
pinctrl-1 = <&i2s2_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN i2s2 */
clocks = <&rcc SPI2>, <&rcc SPI2_K>, <&rcc PLL3_Q>, <&rcc PLL3_R>;
clock-names = "pclk", "i2sclk", "x8k", "x11k";
i2s2_port:port{
i2s2_endpoint:endpoint{
remote-endpoint = <&sii9022_tx_endpoint>;
dai-format = "i2s";
mclk-fs = <256>;
};
};
/* USER CODE END i2s2 */
};