Uboot Environment Configuration
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-08 2:21 AM - last edited on 2023-07-13 8:13 AM by Kevin HUBER
Hello,
i am using an stm32mp1-dk2 board.
For using fw_printenv and other uboot tools from user space one must define a "/etc/fw_env.config" file. I can see that the "/uboot.env" file is driectly saved under the root "/" and so i defined the "fw_env.config" like that:
# cat /etc/fw_env.config
# Device name Device offset Env. size Flash sector size
/uboot.env 0x0000 0x2000
But every time i run fw_printenv i get following msg:
# fw_printenv
Warning: Bad CRC, using default environment
bootcmd=bootp; setenv bootargs root=/dev/nfs nfsroot=${serverip}:${rootpath} ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off; bootm
bootdelay=5
baudrate=115200
As you can it claims about "BAD CRC...".
My question is:
How should a correct "fW_env.config" looks like for a stm32mp1-dk2 board?
Thanks
- Labels:
-
STM32MP15 Lines
-
U-Boot
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-23 1:10 AM
Hello @ajava ,
This issue is known and will be fixed in the next release MMDV-2.0.0.
Here is the patch in u-boot to fix the CRC error:
The output of the function mmc_offset_try_partition must be a
byte offset in mmc and not a multiple of blksz.
This function is used in mmc_offset(), called by mmc_get_env_addr()
and the offset is used in write_env(), erase_env() and read_env().
In these function, blk_start = offset / mmc->read_bl_len
or /write_bl_len so this offset is not a multiple of blksz.
Signed-off-by: Patrick Delaunay <patrick.delau...@st.com>
---
env/mmc.c | 4 ++--
1 file changed, 2 insertions(+), 2 deletions(-)
diff --git a/env/mmc.c b/env/mmc.c
index 902cca23ad..c24b169f3e 100644
--- a/env/mmc.c
+++ b/env/mmc.c
@@ -56,10 +56,10 @@ static inline int mmc_offset_try_partition(const char *str,
s64 *val)
}
/* round up to info.blksz */
- len = (CONFIG_ENV_SIZE + info.blksz - 1) & ~(info.blksz - 1);
+ len = DIV_ROUND_UP(CONFIG_ENV_SIZE, info.blksz);
/* use the top of the partion for the environment */
- *val = (info.start + info.size - 1) - len / info.blksz;
+ *val = (info.start + info.size - len) * info.blksz;
return 0;
}
--
2.17.1
BR,
Christophe
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-23 7:02 AM
thanks @Christophe Guibout i just applied the patch, but unfortunately i still get the Bad-CRC Error! the problem is i am not realy sure if my fw_env.config-setting is really ok.
# cat /etc/fw_env.config
# Device name Device offset Env. size Flash sector size
/uboot.env 0x0000 0x2000
But unfortunately there is alno no where documented how to setup this file for STM32mp1-boards, where the uboot.env-file os saved directly under root "/" of ext4 partition!
any suggestion is welcome!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-24 1:40 AM
Hi @ajava ,
Your fw_env.config looks good.
Our new fw_env.config file would not help because in the next release, u-boot-env will move at the end of ssbl partition.
Maybe there is a dependency on the patch, like this one : https://www.mail-archive.com/u-boot@lists.denx.de/msg360710.html
The last patch shouldn't help, but I mention it for information : https://www.mail-archive.com/u-boot@lists.denx.de/msg360708.html
We use to upstream patches, so feel free to look into the following new patches related to env : https://www.mail-archive.com/search?l=u-boot%40lists.denx.de&q=%40st.com+env&x=0&y=0
Hope it will help.
BR,
Christophe
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-24 3:10 AM
@Christophe Guibout thanks, so i think it is better to wait till your patches are in official release.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-24 6:24 AM
@Christophe Guibout to satisfy my own curiosity, i also tried the other patches of the patch-series (1-3) you mentioned. But unfortunately i am still getting CRC-Error :(
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-28 3:45 PM
in Open ST Linux v1.2.0 U-Boot enviromnent is saved at root (/) of bootfs (4th parttion of SD card)
normally mounted in /boot directory in Linux
Board $> mount /dev/mmcblk0p4 /boot (if not already done)
Can you try with: /boot/uboot.env
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-05-28 9:50 PM
Hai,
I was also trying to include the fw_printenv in the user space but when I include u-boot-fw-utils in my st-image-core.bb file I was throwing the exception as below
ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at yocto-stm32mp1-koan/build/tmp-glibc/work/stm32mp1_disco-openstlinux_weston-linux-gnueabi/u-boot-fw-utils/1_2018.07-r0/temp/log.do_compile.28043)
ERROR: Task (yocto-stm32mp1-koan/sources/poky/meta/recipes-bsp/u-boot/u-boot-fw-utils_2018.07.bb:do_compile) failed with exit code '1'
Can you tell me how to include the fw-utils in the build and I am working on STM32MP157C-DK2 board.
Regards
Srikanth.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-03 6:38 AM
@Christophe Guibout
Ok, I am now using the latest release, where "uboot-env" is saved at the end of uboot-image partition (mmcblk0p3).
This relase: https://github.com/STMicroelectronics/u-boot
Regarding the config-file, the env-settings are:
So I configured the "/etc/fw_env.config":
# MTD device name Device offset Env. size Flash sector size
/dev/mmcblk0p3 0x280000 0x2000 0x40000
But unfortunately it is still no working and gives "CRC"-Erorr!
What is going wrong here? Why?
Thanks and Regards
Arash
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-07-27 8:49 PM
@ajava@Christophe Guibout,
Any update on this issue with latest release of OpenSTLinux, i'm still seeing the same "Warning: Bad CRC, using default environment" with STM32MP135-DK board