to complete : each MMC partition needs to be aligned on MMC erase blockhttps://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#GPT_partition_sizesFor FIP: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#NOR_Flash_memory_an...
For information,in U-Boot for V2.0, "@Name" with full SOC name is provide during USB enumeration: Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157CAA Rev.B,but this field is compatible only with the latest ST...
Hi Adrian,I don't understood extlinux.conf refence here....it is not used for STM32CubeProgrammer load.To start your custom device tree for U-Boot based on DK2 :cp arch/arm/dts/stm32mp157c-dk2.dts arch/arm/dts/stm32mp157-custom.dtsit is the kernel de...
Hi,with OpenSTLinux V2.0.0, it is now possible to load and execute a Linux kernel in RAM with STM32CubeProgrammerhttps://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#FlashLayout_file_to_load_and_start_kernel#Opt Id Name Type IP Offset...
in Open ST Linux v1.2.0 U-Boot enviromnent is saved at root (/) of bootfs (4th parttion of SD card)normally mounted in /boot directory in LinuxBoard $> mount /dev/mmcblk0p4 /boot (if not already done)Can you try with: /boot/uboot.env