2020-09-11 12:56 AM
hi
i am using stm32mp157caa3, there is a i2c slave operating at 3v3, while design, we have not connected( "forget")pull up line on i2c clk and data line,
so i tried enabling open-drain internal pull up in dtsi , but i2cdetect is not able to find the slave device
dtsi :
pins {
pinmux = <STM32_PINMUX('H', 11, AF5)>, /* I2C1_SCL */
<STM32_PINMUX('B', 9, AF4)>; /* I2C1_SDA */
bias-pull-up;
drive-open-drain;
slew-rate = <1>;
};
let me if my configuration and understanding is right ?
2020-09-11 2:01 AM
Hi @ARa.1
we had hard time not using external pull-ups.
If you try to look up for exact resistance in the datasheet then you do not find information.
I assume the "pullup" is implemented as current sink.
I recommend you to use external pullup resistor 2kOhm.
HTH, Adib.
--
2021-03-07 9:35 AM
hello, did it work?
2021-03-07 9:51 AM
Did what work? Using the internal pull-ups is unlikely to be satisfactory/reliable.
Tack on 2K7 pull-up resistors to some accessible points for the SDA and SCL signals.
2021-03-07 11:16 AM
For on-board low connection with capacitve load, internal pull up may work work in many case.
2021-03-08 1:37 AM
Hello Uwe,
may and should are not sufficient when things are REQUIRED.
The "pull up" is a current source and thus not guaranteed to have a specific resistance.
There is no confirmed information in the datasheet about that.
If you really depend on I2C you must add external pull up resistors.
HTH, Adib.
--
2021-03-08 3:37 AM
With STM32 parts, internal pull-ups hardly ever worked for I2C.
They are about one order of magnitude to large (high impedance).
I don't expect it any different for the MP.
2021-03-12 8:47 AM
Hi,
just to clarify, pull-up and pull-down values are stated in datasheet (e.g. DS12505), please look at "I/O static characteristics" table.
Value if 40kOhm typical (between 25K and 50K).
I confirm that the internal pull-up is too large for usual I2C (with 50K/30pF load, you might barely reach 100KHz).
I agree, the I2C recommended pull-up is not in STM32 datasheet, but useful and complete information on Rp could be found in I2C standard.
As stated, rule of thumb using 2.7K pull-ups work fine.
Regards.