ā2021-09-30 07:48 AM
I just got my STM32WB55 Nucleo boards with FUS v.0.5.3 and trying to upgrade firmware but neither of the provided .bin files in "repository" ("stm32wb5x_FUS_fw.bin" or "stm32wb5x_FUS_fw_for_fus_0_5_3.bin") work. I get the same message for both when trying to program the files using STM32CubeProgrammer tool. (Note: message "Firmware Delete Successful" was present).
Attaching a picture of the error message I get.
Note: I tried to accomplish the same thing using both user USB DFU and ST-LINK interfaces.
Here's log from my flash attempts:
10:43:51 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
10:43:51 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
10:43:51 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
10:43:51 : Warning: Option Bytes are unchanged, Data won't be downloaded
10:43:51 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
10:43:51 : Memory Programming ...
10:43:51 : Opening and parsing file: 0x495_FUS_Operator.bin
10:43:51 : File : 0x495_FUS_Operator.bin
10:43:51 : Size : 8 KBytes
10:43:51 : Address : 0x08000000
10:43:51 : Erasing memory corresponding to segment 0:
10:43:51 : Erasing internal memory sectors [0 1]
10:43:51 : Download in Progress:
10:43:51 : File download complete
10:43:51 : Time elapsed during download operation: 00:00:00.292
10:43:51 : Application is running, Please Hold on...
10:43:51 : Reconnecting...
10:43:51 : Reconnected !
10:43:52 : FUS_STATE_IDLE
10:43:52 : Read FUS state command execution finished
10:43:52 : UPLOADING ...
10:43:52 : Size : 4 Bytes
10:43:52 : Address : 0x20010010
10:43:52 : Read progress:
10:43:52 : Data read successfully
10:43:52 : Time elapsed during the read operation is: 00:00:00.000
10:44:29 : Option byte command : -ob nSWBOOT0=1
10:44:29 : PROGRAMMING OPTION BYTES AREA ...
10:44:29 : Bank : 0x00
10:44:29 : Address : 0x58004020
10:44:29 : Size : 96 Bytes
10:44:29 : Reconnecting...
10:44:35 : Reconnected !
10:44:35 : UPLOADING OPTION BYTES DATA ...
10:44:35 : Bank : 0x00
10:44:35 : Address : 0x58004020
10:44:35 : Size : 96 Bytes
10:44:35 : Bank : 0x01
10:44:35 : Address : 0x58004080
10:44:35 : Size : 8 Bytes
10:44:35 : OPTION BYTE PROGRAMMING VERIFICATION:
10:44:35 : Option Bytes successfully programmed
10:44:46 : Old Firmware delete ...
10:44:46 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
10:44:46 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
10:44:46 : Reconnecting...
10:44:51 : Reconnected !
10:44:51 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
10:44:51 : Memory Programming ...
10:44:51 : Opening and parsing file: 0x495_FUS_Operator.bin
10:44:51 : File : 0x495_FUS_Operator.bin
10:44:51 : Size : 8 KBytes
10:44:51 : Address : 0x08000000
10:44:51 : Erasing memory corresponding to segment 0:
10:44:51 : Erasing internal memory sectors [0 1]
10:44:51 : Download in Progress:
10:44:51 : File download complete
10:44:51 : Time elapsed during download operation: 00:00:00.292
10:44:51 : Application is running, Please Hold on...
10:44:58 : Reconnecting...
10:44:58 : Reconnected !
10:44:58 : Warning: FUS_STATE_IMG_NOT_FOUND, Flash already empty !
10:45:00 : Firmware delete Success
10:45:00 : Download Stack/FUS image at address 0x803a000 ...
10:45:00 : Memory Programming ...
10:45:00 : Opening and parsing file: stm32wb5x_FUS_fw_for_fus_0_5_3.bin
10:45:00 : File : stm32wb5x_FUS_fw_for_fus_0_5_3.bin
10:45:00 : Size : 24492 Bytes
10:45:00 : Address : 0x0803A000
10:45:00 : Erasing memory corresponding to segment 0:
10:45:00 : Erasing internal memory sectors [58 63]
10:45:00 : Download in Progress:
10:45:00 : File download complete
10:45:00 : Time elapsed during download operation: 00:00:00.666
10:45:00 : Firmware Upgrade process started ...
10:45:00 : Application is running, Please Hold on...
10:45:12 : Reconnecting...
10:45:12 : Reconnected !
10:45:12 : Error: FUS_STATE_IMG_NOT_AUTHENTIC
Solved! Go to Solution.
ā2021-10-01 07:13 AM
Try setting RDP option byte to 0xBB and then back to 0xAA.
Then try to upgrade the FUS once again.
Hope this helps you !
ā2021-10-01 06:58 AM
Hello @AOris.1ā,
It maybe the error caused by the previous FW installation.
Make sure to perform a partial mass erase of the flash memory and ensure a clean memory before any programming.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
ā2021-10-01 07:06 AM
Imen,
ā
Thank you for the response but I must say that I have already tried that and yet still same error.ā
ā2021-10-01 07:13 AM
Try setting RDP option byte to 0xBB and then back to 0xAA.
Then try to upgrade the FUS once again.
Hope this helps you !
ā2021-10-04 07:57 AM
Hi @AOris.1ā ,
There is step by step mentioned in FW release note describing how to upgrade/install the FUS :
How to flash the Wireless Coprocessor Binary via SWD/JTAG by ST-LINK (STM32CubeProgrammer GUI)
Can you please try it and tell me if it is OK ?
Houda
ā2021-10-04 08:08 AM
Houda,
good points but I've been through those already... Here's the log:
11:02:39 : STM32CubeProgrammer API v2.8.0
11:03:11 : ST-LINK SN : 066BFF485651836687021822
11:03:11 : ST-LINK FW : V2J38M27
11:03:11 : Board : P-NUCLEO-WB55
11:03:11 : Voltage : 3.24V
11:03:11 : SWD freq : 4000 KHz
11:03:11 : Connect mode: Normal
11:03:11 : Reset mode : Software reset
11:03:11 : Device ID : 0x495
11:03:11 : Revision ID : Rev Y
11:03:11 : Debug in Low Power mode enabled.
11:03:11 : UPLOADING OPTION BYTES DATA ...
11:03:11 : Bank : 0x00
11:03:11 : Address : 0x58004020
11:03:11 : Size : 96 Bytes
11:03:11 : Bank : 0x01
11:03:11 : Address : 0x58004080
11:03:11 : Size : 8 Bytes
11:03:11 : UPLOADING ...
11:03:11 : Size : 1024 Bytes
11:03:11 : Address : 0x8000000
11:03:11 : Read progress:
11:03:11 : Data read successfully
11:03:11 : Time elapsed during the read operation is: 00:00:00.007
11:03:23 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
11:03:23 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
11:03:23 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
11:03:23 : Warning: Option Bytes are unchanged, Data won't be downloaded
11:03:23 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
11:03:23 : Memory Programming ...
11:03:23 : Opening and parsing file: 0x495_FUS_Operator.bin
11:03:23 : File : 0x495_FUS_Operator.bin
11:03:23 : Size : 8 KBytes
11:03:23 : Address : 0x08000000
11:03:23 : Erasing memory corresponding to segment 0:
11:03:23 : Erasing internal memory sectors [0 1]
11:03:24 : Download in Progress:
11:03:24 : File download complete
11:03:24 : Time elapsed during download operation: 00:00:00.284
11:03:24 : Application is running, Please Hold on...
11:03:24 : Reconnecting...
11:03:24 : Reconnected !
11:03:28 : Reconnecting...
11:03:28 : Reconnected !
11:03:29 : StartFus activated successfully
11:03:29 : FUS_STATE_IDLE
11:03:29 : Start FUS execution finished
11:03:41 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
11:03:41 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
11:03:41 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
11:03:41 : Warning: Option Bytes are unchanged, Data won't be downloaded
11:03:41 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
11:03:41 : Memory Programming ...
11:03:41 : Opening and parsing file: 0x495_FUS_Operator.bin
11:03:41 : File : 0x495_FUS_Operator.bin
11:03:41 : Size : 8 KBytes
11:03:41 : Address : 0x08000000
11:03:41 : Erasing memory corresponding to segment 0:
11:03:41 : Erasing internal memory sectors [0 1]
11:03:42 : Download in Progress:
11:03:42 : File download complete
11:03:42 : Time elapsed during download operation: 00:00:00.286
11:03:42 : Application is running, Please Hold on...
11:03:42 : Reconnecting...
11:03:42 : Reconnected !
11:03:43 : FUS_STATE_IDLE
11:03:43 : Read FUS state command execution finished
11:03:43 : UPLOADING ...
11:03:43 : Size : 4 Bytes
11:03:43 : Address : 0x20010010
11:03:43 : Read progress:
11:03:43 : Data read successfully
11:03:43 : Time elapsed during the read operation is: 00:00:00.001
11:05:04 : Old Firmware delete ...
11:05:04 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
11:05:04 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
11:05:04 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
11:05:04 : Warning: Option Bytes are unchanged, Data won't be downloaded
11:05:04 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
11:05:04 : Memory Programming ...
11:05:04 : Opening and parsing file: 0x495_FUS_Operator.bin
11:05:04 : File : 0x495_FUS_Operator.bin
11:05:04 : Size : 8 KBytes
11:05:04 : Address : 0x08000000
11:05:04 : Erasing memory corresponding to segment 0:
11:05:04 : Erasing internal memory sectors [0 1]
11:05:04 : Download in Progress:
11:05:04 : File download complete
11:05:04 : Time elapsed during download operation: 00:00:00.289
11:05:04 : Application is running, Please Hold on...
11:05:11 : Reconnecting...
11:05:11 : Reconnected !
11:05:11 : Warning: FUS_STATE_IMG_NOT_FOUND, Flash already empty !
11:05:13 : Firmware delete Success
11:05:13 : Download Stack/FUS image at address 0x803a000 ...
11:05:13 : Memory Programming ...
11:05:13 : Opening and parsing file: stm32wb5x_FUS_fw_for_fus_0_5_3.bin
11:05:13 : File : stm32wb5x_FUS_fw_for_fus_0_5_3.bin
11:05:13 : Size : 24492 Bytes
11:05:13 : Address : 0x0803A000
11:05:13 : Erasing memory corresponding to segment 0:
11:05:13 : Erasing internal memory sectors [58 63]
11:05:13 : Download in Progress:
11:05:13 : File download complete
11:05:13 : Time elapsed during download operation: 00:00:00.655
11:05:13 : Firmware Upgrade process started ...
11:05:13 : Application is running, Please Hold on...
11:05:25 : Reconnecting...
11:05:25 : Reconnected !
11:05:25 : Error: FUS_STATE_IMG_NOT_AUTHENTIC
ā2021-10-04 08:15 AM
Imen,
IT WORKED!!!!!!!!!!!!!!!!!!!!! Thank you!!!!
ā2021-10-04 08:16 AM
Can you explain why this works, please?
ā2021-10-04 08:33 AM
Really glad that the issue is solved š
This is a trick to clean the flash that I used before upgrading the board, which helps to sort out from such unexpected situationš
Imen
ā2021-10-04 08:39 AM
Good enough for an answer. I was more interested in the details because I'm suspecting there's a bug in the fw/sw(?) But it's up to the ST engineers to figure that out and "outsiders" shouldn't be involved in the direct resolution process.
Thank you, again.