cancel
Showing results for 
Search instead for 
Did you mean: 

After download the project shuts down.

StephenNic
Associate II

After getting several projects working and starting a new project the following problem occurred at run time.

Returned to previous working projects and get same result.

 

STMicroelectronics ST-LINK GDB server. Version 7.9.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : EnableWaiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.18.0

-------------------------------------------------------------------

Log output file: C:\Users\want2\AppData\Local\Temp\STM32CubeProgrammer_a21344.log

ST-LINK SN : 066FFF575487884867140827

ST-LINK FW : V2J45M31

Board : NUCLEO-F767ZI

Voltage : 3.25V

SWD freq : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x451

Revision ID : Rev Z

Device name : STM32F76x/STM32F77x

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7

BL Version : 0x93

 

Opening and parsing file: ST-LINK_GDB_server_a21344.srec

Memory Programming ...

File : ST-LINK_GDB_server_a21344.srec

Size : 84.70 KB

Address : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 2]

Download in Progress:

 

File download complete

Time elapsed during download operation: 00:00:01.679

 

Verifying ...

 

Download verified successfully

 

Shutting down...

Exit.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

The "Shutting down..." message is from the GDB server program on your computer shutting down, because it's done uploading the program to the board, verified it's correct, and isn't needed anymore.

The program on the board is running.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

5 REPLIES 5
TDK
Super User

The "Shutting down..." message is from the GDB server program on your computer shutting down, because it's done uploading the program to the board, verified it's correct, and isn't needed anymore.

The program on the board is running.

If you feel a post has answered your question, please click "Accept as Solution".

It appears that when I started a new project the previous projects changes and additions were lost as those files were restored to their original contents from STMicroelectronics libraries..... Obviously, I selected something incorrectly or failed to select something correctly... Hopefully I explained my issue clearly.... What is the something I need to do or not do that prevents the changes and additions on previous projects from being erased or file being overwritten?

In generated code files, you can only put code within USER CODE BEGIN and USER CODE END blocks. Otherwise, it will be erased on regeneration.

If you feel a post has answered your question, please click "Accept as Solution".

No, your not understanding the problem.... I religiously follow the USER CODE BEGIN and USER CODE END block guidelines..... let me try to explain in a different way.

Project A is created from downloaded libraries, updated, and tested successfully after mulitiple code changes, compiling processes, and debug cycles.

Then on to Project B which is created from new set of downloaded files which are the same libraries project A started from but modified for a different application.

After modifying project B files, compiling, downloading to development board, debugging, and successfully testing, I return to project A to find all modified files retored to original state.

Why? I'm expecting that the two projects are not sharing files or access while working on another project. 

Files don't change on their own. If the projects don't share files, they will be independent.

Must be something else going on there.

 

Looking at file modification times might give you a clue, or file history.

If you feel a post has answered your question, please click "Accept as Solution".