2020-12-10 11:10 AM
I'm not able to connect the
NUCLEO-STM32WL55JC1 board (Updated FW today to V3.J7) to the
STM32CubeMonitor V.1.1.0
Fun facts: Blink connection test works and the firmware is reported correctly in the connection config box.
Error message reads: "not connected | JTAG/SWD error/f5)
In addition: Please fix the copy & paste bug of the Mac version (1.1.0). Known for at least 8 months.
Solved! Go to Solution.
2020-12-11 1:35 AM
Hello Franck
Many STM32WL examples disable the debug port and enable sleep mode. This is good to optimize power/security,but STM32CubeMonitor is then not allowed to connect with SWD. (I have tested with LoRaWan_AT_Slave)
To have a stable debug connection, the debug must be enabled and sleep disabled :
For this example, in in the file sys_conf.h,
The connection should work.
Let us know if you are able to connect, it can be useful information for many users.
Best regards
Stephane
2020-12-11 1:35 AM
Hello Franck
Many STM32WL examples disable the debug port and enable sleep mode. This is good to optimize power/security,but STM32CubeMonitor is then not allowed to connect with SWD. (I have tested with LoRaWan_AT_Slave)
To have a stable debug connection, the debug must be enabled and sleep disabled :
For this example, in in the file sys_conf.h,
The connection should work.
Let us know if you are able to connect, it can be useful information for many users.
Best regards
Stephane
2020-12-11 9:25 AM
Hallo Stephane,
thank you. This was the correct answer.
Regards, Frank