Skip to main content
Visitor II
August 30, 2024
Question

STM32WL55JC LoRaWAN Working Only on Dual-Core for FUOTA

  • August 30, 2024
  • 1 reply
  • 721 views

I'm working on a project with the STM32WL55JC microcontroller. Before testing the LoRaWAN_FUOTA_DualCore application, my LoRaWAN setup was functioning correctly with all example applications.

However, after flashing the LoRaWAN_FUOTA_DualCore application, I noticed that only this application is working. While other applications like LoRaWAN_FUOTA, LoRaWAN_End_Node, and LoRaWAN_End_Node_DualCore are functional in terms of peripherals, my device is unable to connect to the LoRa gateway.

Could you help me understand why it’s only working with the LoRaWAN_FUOTA_DualCore application?

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
October 14, 2024

Hello @karthiksb 

I'm not able to reproduce that issue. Could you please tell me how you have reproduced that.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.