STM32WBA52 programming on custom board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-19 5:45 AM - edited ‎2024-11-19 11:53 PM
I am trying to detect my stm32wba52cg bare chip with my developed custom PCB board with onboard stlink as external programmer from a discoveryboard but its showing this msg-
Can not connect to target!
Please select "Connect Under Reset" mode from Target->Settings menu and try again.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
No target connected.
this are my connection for programming my wba52 controller-
discovery stlink stm32wba52
swdio swdio
swclk swclk
nrst rst
3.3 (from discovery board) 3.3
gnd gnd
Below is my schematic attached:
I have exposed all the pins.
Solved! Go to Solution.
- Labels:
-
STM32WBA series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-20 12:52 AM
Hello @suvendusahux
As I can see on your schematic, you are using the PA13 as SWCLK and PA14 as SWDIO. But as you can see on the Table 24 of the DS14127, PA14 is the SWCLK pin and PA13 is the SWDIO pin:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-19 6:02 AM
@suvendusahux wrote:stm32wba52cg bare chip
What do you mean by that - Literally a bare chip; no PCB at all? A custom PCB ? Other?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-19 9:43 AM
A custom pcb with stmwba52.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-19 10:14 AM - edited ‎2024-11-19 11:52 AM
Thanks - I updated the title to reflect that.
Please post the schematic of your board.
Some good, clear photos of your setup would also help.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-19 11:54 PM
I have attached the schematic above. Please check.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-20 12:52 AM
Hello @suvendusahux
As I can see on your schematic, you are using the PA13 as SWCLK and PA14 as SWDIO. But as you can see on the Table 24 of the DS14127, PA14 is the SWCLK pin and PA13 is the SWDIO pin:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-02 3:17 AM
I am trying to load the BLE_heartrate_ota example to my wba52 controller I am getting these logs after RUN and DEBUG -
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------
ST-LINK SN : 066DFF555185754867142533
ST-LINK FW : V2J45M30
Board : NUCLEO-F446RE
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x492
Revision ID : Rev A
Device name : STM32WBA52/54/55
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0xB0
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a15024.srec
File : ST-LINK_GDB_server_a15024.srec
Size : 223.95 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 27]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:02.366
Verifying ...
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Shutting down...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-02 3:22 AM - edited ‎2024-12-02 3:22 AM
PA14 is the SWCLK pin and PA13 is the SWDIO pin i swaped the pins and it detected the mcu but I am getting Target is not responding message every time I try to run or debug the BLE_heartrate_ota example for stm32wba52.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-02 10:50 PM
I Tried to connect buttons to my mcu as shown in nucleo board but its not showing in my st ble toolbox when I press B1 connected to PC13.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-02 10:52 PM
These are some logs from usart1 when I press reset button.
==>> Start Ble_Hci_Gap_Gatt_Init function
Success: aci_hal_write_config_data command - CONFIG_DATA_PUBADDR_OFFSET
Public Bluetooth Address: 00:80:e1:2a:b0:9a
Success: aci_hal_write_config_data command - CONFIG_DATA_IR_OFFSET
Success: aci_hal_write_config_data command - CONFIG_DATA_ER_OFFSET
Success: aci_hal_set_tx_power_level command
Success: aci_gatt_init command
Success: aci_gap_init command
Success: aci_gatt_update_char_value - Device Name
Success: aci_gatt_update_char_value - Appearance
Success: hci_le_set_default_phy command
Success: aci_gap_set_io_capability command
Success: aci_gap_set_authentication_requirement command
Success: aci_gap_configure_whitelist command
==>> End Ble_Hci_Gap_Gatt_Init function
Services and Characteristics creation
Success: aci_gatt_add_service command: P2P_Server
Success: aci_gatt_add_char command : LED_C
Success: aci_gatt_add_char command : SWITCH_C
Success: aci_gatt_add_service command: OTA
Success: aci_gatt_add_char command : BASE_ADR
Success: aci_gatt_add_char command : CONF
Success: aci_gatt_add_char command : RAW_DATA
End of Services and Characteristics creation