2024-07-01 08:01 AM
Hi everyone,
We recently purchased a NUCLEO-WB55RG Dual Core EVK for R&D purposes. We later realized that in the STM32WB55CGU6TR MCU, the Cortex M0+ core is dedicated to BLE. Is there any possibility of toggling GPIO on the Cortex M0+ core? If so, can anyone share a sample code for this?
Thanks in advance!
Solved! Go to Solution.
2024-07-01 08:29 AM
Hello @pippalla_chakravarthi
CM0+ is a closed system really dedicated to Wireless Stack. So, you can't use it for other purpose.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-01 08:25 AM
Too what end?
The TIM peripherals can toggle pins associated with them, with no user intervention.
You should be able to do TIM+DMA+GPIO to output a pattern file to pin(s) on a single GPIOx bank
2024-07-01 08:29 AM
Hello @pippalla_chakravarthi
CM0+ is a closed system really dedicated to Wireless Stack. So, you can't use it for other purpose.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-01 09:15 AM
Thanks for the reply, @STTwo-32
I'm working on generating two different trigger signals: one at 60Hz and another at 600Hz, using three PWM signals on three GPIO or timer channels. I attempted to use slave trigger mode for synchronization, but I'm encountering a phase shift in the PWM signals after two or three pulses.
Can you please guide me on the best possible way to achieve this task?
2024-07-01 09:28 AM - edited 2024-07-01 09:28 AM
That sounds like a new question.
Best to mark the solution here, and then start a new thread for the new question.
Post a reply here with a link to the new thread.
2024-07-01 09:48 AM
Hi @Andrew Neil ,
I am closing this thread and opened new thread
Here is the new thread link FYR : Generating 60Hz and 600Hz Trigger Signals with PWM in STM32WB55CGU6TR : Synchronization Issue in Slave Mode
Thanks in advance.