2021-08-28 01:29 PM
From the STM32CubeWB firmware package, there is a Thread_RCP project. However, there doesn't seem to be any documentation for it (it is not even mentioned in AN5289). The only hint is the readme.txt file which says:
"This application is used to demonstrate the OpenThread Border router feature using an STM32WB device.
To play with the demo, you need a Raspberry Pi 3B (RPi) to perform the link with Wi-Fi/Ethernet networks
The full setup and the associated documentations can be requested to ST on demand".
Where can I find the full setup and associated documentation?
Thank you,
2022-11-19 10:29 PM
@Remi QUINTIN
Appreciated if you can advise on this?
2022-11-20 07:53 AM
the document has 13 pages; just download it . 🙂
2022-11-20 04:01 PM
The documentation says this, so I'm asking.
A full configured RPi image is provided by ST.
Please get the OTBR_CLI_RPi_1.0.img.
Regards
2022-11-20 04:02 PM
2024-02-07 12:33 PM
I'm also looking for the OTBR_CLI_RPi_1.0.img downloading sources for my students (educational HE project).
Is there any info I'm missing? All documentation links stating "get ... file" are inactive.
Best regards,
Piotr