2017-06-12 6:37 AM
Hello,
I am trying to use LoRa connectivity with the brand new b-l072z-lrwan1 discovery board. The End Node project works perfectly but I have an issue with the AT Slave project. When I try to send LoRa packet to my Multitech gateway, this one never receive the packet and I cannot use AT command with the disco board anymore. I can only do a hardware reset of the board.
As you can see on my screenshot, the Join process has been done correctly. After the AT+SEND command I never receive a status like OK or AT ERROR.
Are you able to help me ?
Thank you !
Aaron
#b-l072z-lrwan1 #at_slave #lora2017-08-16 7:12 PM
I'd suppose using the full sscanf() library would work fine too, the LoRa stack already drags in the entire floating point library already.
Not sure if Keil has this problem, the builds posted reportedly work.
2017-08-16 9:21 PM
Keil built US915 HYBRID version
Added a build with the native sscanf/sprintf libraries
________________ Attachments : LoraDisco_ATSlave_US915HYBRID_FULL_NOT_TINY_V111.hex.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyU2&d=%2Fa%2F0X0000000b8c%2F6osLq0uMI.A_1M7FMrvPaQE9yUBQl4lfGoZDqBDFI3g&asPdf=falseLoraDisco_ATSlave_US915HYBRID_V111.hex.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyUa&d=%2Fa%2F0X0000000b8b%2FH5OQbl_fO3m2yWJPIJLAZdj6EkT4OGY3_oUfo5Zw6VA&asPdf=false2017-08-16 9:44 PM
There is a width issue with the sscanf here in lora.c related to AT+SEND
LoRaMacStatus_t lora_send(const char *buf, unsigned bufSize, unsigned binary)
{ uint8_t appport; /* read and set the application port */ if (1 != sscanf(buf, '%u:', &appport)) { PRINTF('AT+SEND without the application port'); return LORAMAC_STATUS_PARAMETER_INVALID; }2017-08-16 10:10 PM
Yea, I 've also traced to this part which causing the issue.
Modifying the data type of the variable '
appport' from
uint8_t to uint32_t solves it.
Thanks you guys for all the inputs!