2025-02-18 3:48 AM
Hello,
I'm trying to make an OnOff Switch emitter using zigbee on the STM32WB55 Nucleo Board. I started my project from the Zigbee_OnOff_Client_Distrib applications exemple.
The receiver that I use is not made to send back APS ACK. Because of this I add problems with Toggle command on the OnOff ZCL Cluster because the emitter was sending frame retries.
I figured out that I could disable Ack requirement in the APS Frame Control using
zigbee_app_info.onOff_client_1->txOptions &= ~(ZB_APSDE_DATAREQ_TXOPTIONS_ACK);after cluster allocation.
Now, my problem is with the Zdo. In the find and bind process, I send a Simple Descriptor Request:
// /** Simple_Desc_req */
// struct ZbZdoSimpleDescReqT {
// uint16_t dstNwkAddr; /**< Destination network address */
// uint16_t nwkAddrOfInterest; /**< NWKAddrOfInterest */
// uint8_t endpt; /**< Endpoint */
// };
// Request simple descriptor
struct ZbZdoSimpleDescReqT req_simple_desc;
req_simple_desc.dstNwkAddr = zigbee_app_info.SW1_endpoint_bind.nwkAddr;
req_simple_desc.nwkAddrOfInterest = zigbee_app_info.SW1_endpoint_bind.nwkAddr;
req_simple_desc.endpt = zigbee_app_info.SW1_endpoint_bind.endpoint;
ZbZdoSimpleDescReq(zigbee_app_info.zb, &req_simple_desc, simple_desc_response_cb, NULL);when I check in the packet with a sniffer, I see that the Ack requirement in the APS Frame Control is set, and the emitter send frame retries.
My questions are :
- How can I disable Ack requirement in the APS Frame Control for zdo requests?
- Is there a way to configure the APS Layer globally?
Thank you,
Solved! Go to Solution.
2025-02-19 8:15 AM
Hello @Nath,
Thanks for contacting us.
Please find my answers to your questions:
Please find the paragraph from Zigbee spec :
Kind regards,
Ouadi
2025-02-19 8:15 AM
Hello @Nath,
Thanks for contacting us.
Please find my answers to your questions:
Please find the paragraph from Zigbee spec :
Kind regards,
Ouadi
2025-02-20 12:00 AM
Hello @Ouadi,
Thank you for your answers.