Posted on August 17, 2017 at 05:10Yea, I 've also traced to this part which causing the issue.Modifying the data type of the variable 'appport' from uint8_t to uint32_t solves it.Thanks you guys for all the inputs!
Posted on August 16, 2017 at 04:21Thanks Clive One. Your build works for me. I can send the data and receive response.But I also need to figure out our cause as we need to customize the firmware and build ourselves.
Posted on August 15, 2017 at 12:12I have exactly the same problem in the AT_Slave software that I built.I was using LRWAN software v1.1.1. I only added the 'REGION_US915' compiler switch without modifying anything of the code.If I use the binary pro...