2019-10-18 3:58 AM
Hi!
I'm trying to enable the PDM interface on a STM32WB55RGV with one microphone. Basically i followed the AN5027 application note, but I'm not able to start the clock on the proper GPIO.
The configuration from CUBE-MX seems ok, and I checked the registers value, so maybe I'm setting up the wrong API to start the streaming.
Any advice?
MX_SAI1_Init();
osDelay(10);
//HAL_SAI_Receive_DMA(&hsai_BlockA1, (uint8_t *)mic_buff, MIC_BUFF_LEN);
HAL_SAI_Receive(&hsai_BlockA1, (uint8_t *)mic_buff, MIC_BUFF_LEN, 100);
/* start application */
while (1){
osDelay(1000);
}
Solved! Go to Solution.
2019-10-21 9:35 AM
Thanks waclawek.jan
The issue comes from the RCC, selecting the PLLP clock source instead of PLLSAI1 the PDM peripheral works. It seems an CUBEMX bug generating the RCC config function.
2019-10-18 4:57 AM
How is SAI clock set in RCC?
Read out and check/post content of relevant RCC, SAI and GPIO registers.
JW
2019-10-18 7:41 AM
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 8;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV31;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
|RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
/** Initializes the peripherals clocks
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS|RCC_PERIPHCLK_SAI1
|RCC_PERIPHCLK_I2C1|RCC_PERIPHCLK_I2C3
|RCC_PERIPHCLK_ADC;
PeriphClkInitStruct.PLLSAI1.PLLN = 6;
PeriphClkInitStruct.PLLSAI1.PLLP = RCC_PLLP_DIV31;
PeriphClkInitStruct.PLLSAI1.PLLQ = RCC_PLLQ_DIV2;
PeriphClkInitStruct.PLLSAI1.PLLR = RCC_PLLR_DIV2;
PeriphClkInitStruct.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_SAI1CLK;
PeriphClkInitStruct.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1;
PeriphClkInitStruct.I2c3ClockSelection = RCC_I2C3CLKSOURCE_PCLK1;
PeriphClkInitStruct.Sai1ClockSelection = RCC_SAI1CLKSOURCE_PLLSAI1;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL;
PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSI;
PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
2019-10-18 7:54 AM
I don't use Cube and don't understand its gibberish.
It appears you are using the SAI PLL's output - is that PLL running? Maybe there's no simple way to test that on your STM32 model, then use for SAI for testing a clock you are sure it's running.
Read out and check/post content of relevant RCC, SAI and GPIO registers.
JW
2019-10-18 8:05 AM
Thank you su much.
Here the SAI registers:
The RCC :
and lastly the GPIOs configuration:
PA10 is the SAI_D1 and PA8_SAI1_CK2
2019-10-18 9:13 AM
OK and GPIO_AFRx is set to the appropriate AF?
I have no experience with SAI with PDM, so you may want to check that yourself against the RM.
Did you make sure there is a valid clock input in RCC, maybe switching to a clock source which is known working (such as the main PLL)?
JW
2019-10-21 9:35 AM
Thanks waclawek.jan
The issue comes from the RCC, selecting the PLLP clock source instead of PLLSAI1 the PDM peripheral works. It seems an CUBEMX bug generating the RCC config function.
2019-10-21 12:29 PM
OK so problem solved? Then please select your post as "Best" to mark the thread as solved.
JW
@Imen DAHMEN - so this appears that CubeMX does not generate code for initializing the PLLSAI for the 'WB55, can this please be checked?
2019-10-28 2:48 AM
Hello @Community member Did you mean by " CubeMX does not generate code for initializing the PLLSAI for the 'WB55" that there's a missed line of code ?
Thanks,
Khouloud
2019-10-28 2:57 AM
and if yes which lignes of code ?
Thanks @Community member
Khouloud