2024-11-26 10:15 AM
Hi ST Experts,
We have a BLE project based on the STM32L476 and HM11 BLE and we are looking to minimize the component count and shrink the board size. We want to replace the STM32L476 with a BLE and MCU single chip solution and we are considering the STM32WB55CGU6, kindly advice the most suitable MCU for a BLE.
We also need a single chip BMS solution with integrated charge controller, protection circuits (Over temperature, over charge/discharge protection etc), Wireless charging (is nice to have), Integrated battery gauge with I2C interface (to read out battery State of Charge and battery Health).
We would love to schedule a meeting to discuss further our requirements.
Looking forward to your response.
Regards,
Paul.
2024-11-26 10:24 AM
@PN_ wrote:We also need a single chip BMS solution
Would need more details - what size & type of battery, etc ...
@PN_ wrote:We would love to schedule a meeting to discuss further our requirements.
Sounds like you want an FAE?
to contact ST direct, see: https://ols.st.com/s/
Or maybe try your local distributor: https://www.st.com/content/st_com/en/contact-us.html
2024-11-26 12:39 PM
Thanks for your response.
So for the battery, we are looking at a 3.7V Li-Po/L-ion battery. The capacity can be up to 5000mah.
And yes we'll like to talk to a field application engineer.
2024-11-26 02:43 PM
Start with the people you're buying from currently..
Find your local sales office, or rep.
2024-11-27 12:57 AM
@PN_ wrote:And yes we'll like to talk to a field application engineer.
Contact details in previous reply.