cancel
Showing results for 
Search instead for 
Did you mean: 

Readout protection of OBK-Keys from user software

Heinz_Baumer
Associate

Hello.

If i set the product state to CLOSED (0x72)  without TZ-enabled (TZEN: 0xC3),

i can't access the device and the OBK-Keystore from outside.

But if i write a user program, i can read the whole OBK-Keystore at:
FLASH_OBK_BASE_S + 0x0100;

So perhaps it is possible to get access to the device with this information.

 

Is there a easy way to protect a read access to the OBK-Key, without using the TZ ?

0 REPLIES 0