2019-07-27 08:26 AM
Hello,
I bought the P-Nucleo-WB55 kit but I'm having problems running the examples provided.
I have overwritten by mistake the demo firmware available in the P-Nucleo-68 and now I would like to download back the demo firmware again starting from the demo provided.
By looking at the documentation here:
It looks like the demo firmware for the nucleo-68 board should be the P2P_Server_ota. Right?
However, after importing the project in STM32CubeIDE and I open it's properties I get the error I reported below.
Why is the board target not selected? I took it from the STM32Cube_FW_WB_V1.2.0 repository directory.
Can someone help me solving this issue?
Thanks in advance.