cancel
Showing results for 
Search instead for 
Did you mean: 

P-Nucleo-WB55 and X-Nucleo-DRP1M1 compatibility

Nos
Associate

Hi all.

The documentation of DRP1M1 says it can be stacked on top any Nucleo board with UCPD peripheral embedded in their microcontrollers. I don't see UCPD feature in WB55RG so I thought they are not compatible.

However, my supplier is positive that the X-Nucleo-DRP1M1 can be used with P-Nucleo-WB55 so I get a little confused here. In the end, can I use the X-Nucleo-DRP1M1 with the P-Nucleo-WB55?

Thank you.

1 REPLY 1
MROUV.1
ST Employee

Hi Nos,
To use X-NUCLEO-DRP1M1 with TCPP03-M20 in order to perform a Dual Role Port application, the STM32 must embed UCPD controller.
Unfortunately, STM32WB55 series do not embed this controller. I've performed the check using Cube-MX.
Fortunatly, 685 others STM32 embeds UCPD. I hope, you will find the one that corresponds to your needs.
Or, if only type-C SINK or SOURCE limited to 5V - 3A, you can use TCPP01-M12 or TCPP02-M18 and use associated X-NUCLEO-SNK1 or X-NUCLEO-SRC1. Then, resources must be attributed according to the examples on X-CUBE-TCPP.
Best regards,
Mathieu