cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo stm32 wl552jc1 Programming

jtallen5
Associate

Hello, I'm a novice at using this forum and programming stm32 boards, so any advice is appreciated.  My plan is to use two stm32wl552jc1 boards to collect weather data and display at a remote location.  My goal is to learn how to program the stm32 boards while developing this weather data project.   At the beginning here I have several questions.

1. Is the nucleo wl552lc1 the right board to use for this project?

2. Which cube ide should I use?  There are so many it's confusing.

3.  Is there online training available?

4.  What is the best way to learn STM32 programming?

Thanks for your help and advice,

John Allen

 

 

 

1 REPLY 1
STTwo-32
ST Employee

Hello @jtallen5 and welcome to the ST Community.

1) Yes, the NUCLEO-WL55JC is the best board for such a project.

2) I suggest you to use the last version of the STM32CubeIDE as an IDE for your project.

3) Yes, there is a training that should help you on your project. This workshop:  specially the video number 4 should do the job fi you 

4) To start with the STM32 world. I suggest you to use those Wiki pages. and if you need informations you can have a look on google or YouTube and you are always welcome to ask on the Community if it need.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.