cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WLE5 Module JOIN FAILED

ethan2
Associate II

Hi,

I'm doing tests based on the LoRaWAN_AT_Slave. One of the modules often appears tMAC txTimeOut, resulting in JOIN FAILED. Same firmware downloaded, but some devices are working, is there any doubt? Is it a hardware problem?

 

[14:47:35.933]发→◇AT+JOIN=1[14:47:35.965]收←◆1s890:TX on freq 470900000 Hz at DR 0 OK [14:47:39.965]收←◆5s893:MAC txTimeOut +EVT:JOIN FAILED

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

I have finally solved the problem, it is the hardware cause.

Thanks.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @ethan2 

Could you please provide more details. What is the exact module you are using (a third party module or a module based on your own design), what is the code you are using and all your use case details if possible.

Best Reagards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi,

I have finally solved the problem, it is the hardware cause.

Thanks.