2023-06-26 05:14 AM
Hello,
I am trying to build an application on a STM32WLE5JBI6 that could work with confirmed downlinks.
I thought that the LoRaMAC handled this but I could not find any mention of it in the documentation or in the code.
As anyone already implemented it?
I really appreciate any help you can provide.
2023-07-06 07:07 AM
Hello @Aschmider and welcome to ST Community.
The LoRaWAN protocol stack is required to implement confirmed downlinks in your application. Your application can be implemented using the Semtech LoRaWAN protocol stack that is included with the STM32WLE5JBI6. This link may help you.
I hope this is going to be helpful.
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.