Hello @RonNad14 and welcome to ST Community.I suggest you to take a look at the application notes AN5481, AN5406 and AN5554. You will find what you need to solve your Class C problem.Best Regards.Issam
Hello @anandhu_us and welcome to ST Community.To get epoch time, I suggest you to take a look to the .ioc file of the project using CubeMX last version. Go to RTC configuration and change the bin Mode to Free running BCD calender and binary mode. The...
Hello again After verification, is impossible to use RF communication in Range 2. Sytem clock in Range 2 should be under 16MHz but in RF transmittion CPU2 CLOCK must be 32MHz. What means system clock should be 32MHz.Best Regards.Issam
Hello @MichaelMor and welcome to ST Community.I suggest you to:stop the PWM outputs of TIM1 CH1 and TIM2 CH1 and then stop TIM1 CH2 (output compare) .start TIM1 CH2 (output compare) and then start the PWM outputs of TIM1 CH1 and TIM2 CH1.This may ens...