learning lrwan1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-21 7:05 AM
hello im doing a school project using a Nucleo-F411RE with a I-NUCLEO-LRWAN1 expansion, anyone got a good text or video tutorial how i connect the two boards?
im using the stm32cubeide
Solved! Go to Solution.
- Labels:
-
STM32F4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-21 7:51 AM
Hello @JoaoFoonseca and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to refer to the Sub-Ghz Phy examples on the I-CUBE-LRWAN. I should be helpful to understand how it should work. For me, i suggest you to use our STM32 long range product the STM32WL that is an MCU with Sub-Ghz communication features. You can find on YouTube lot of videos that help you working with this product. Even a full STM32CubeWL library for this product. For more details refer to this link.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-21 7:51 AM
Hello @JoaoFoonseca and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I suggest you to refer to the Sub-Ghz Phy examples on the I-CUBE-LRWAN. I should be helpful to understand how it should work. For me, i suggest you to use our STM32 long range product the STM32WL that is an MCU with Sub-Ghz communication features. You can find on YouTube lot of videos that help you working with this product. Even a full STM32CubeWL library for this product. For more details refer to this link.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-22 3:57 AM - edited ‎2024-04-22 4:18 AM
@JoaoFoonseca wrote:a good text or video tutorial how i connect the two boards?
What do you mean by that?
Connecting the boards is easy - the I-NUCLEO-LRWAN1 just plugs into the Adruino sockets of the Nucleo-F411RE.
Note that the I-NUCLEO-LRWAN1 is now classed as Obsolete.
EDIT:
The catch here is that the UART TX & RX on the Arduino D1 & D0 pins is needed for the communication between the Nucleo processor and the USI module on the shield.
Therefore SB13 & SB14 will need to be removed - and this means that you won't have any comms over the ST-Link's Virtual COM Port (VCP).
As @STTwo-32 said, you may be better off with an STM32WL board - or, perhaps the B-L072Z-LRWAN1...
A complex system designed from scratch never works and cannot be patched up to make it work.