cancel
Showing results for 
Search instead for 
Did you mean: 

If the power is cut, is the micro controller use battery power automatically?

KKIM.6
Senior

I'm developing STM32WB55VQ power system but I wonder the microcontroller automatically use battery power or not when Vdd is cut.

 

Is there anybody can explain this?

 

17 REPLIES 17

I have more big issue regarding SMPS in microcontroller.

Can I use the SMPS as AC-DC converter to power microcontroller?

Please keep to one question per thread.

If your question here about battery power is answered, please mark the solution.

"Can I use the SMPS as AC-DC converter to power microcontroller?"

Start a new thread for a new question.

Have you studied the datasheet description of what the SMPS does?

You can always give links between threads for reference.

0693W000008y9fZQAQ.png

@KKIM.6​  " I didn't know that the wb55 can charge battery."

Really? it's clearly stated in the datasheet:

0693W00000QKdHjQAL.pngBut note that's only the backup battery/supercap - not any main system supply battery

Note also this diagram showing the different power domains - ie, what gets powered from which supply pins:

0693W00000QKdIcQAL.png@Community member​ "the Data Sheet, might be worth a review"

+99 !

It seems that many (most?) of @KKIM.6​ questions could be answered by a good study of the datasheet and other documentation

https://www.st.com/en/microcontrollers-microprocessors/stm32wb55rg.html#documentation

My final question is whether the power line below is possible or not.0693W00000QKfCgQAL.png 

If it is possible, I don't need PMIC/battery charger between power receiver and microcontroller.

again, that's all answered in the datasheet.

 From your other Thread:

0693W00000QKfO3QAL.png

KKIM.6
Senior

I wonder what's happen if apply more than 4 V.​

Again, the datasheet tells you that.

The 4V is the Absolute Maximum rating; the datasheet defines that term:

0693W00000QKfYNQA1.png