I have a simple code to run a webserver that toggles LED on STM32 Nucleo. I connect to WiFi using ESP 8266 which works perfectly well. I want to migrate this code to Sensortile which uses STM32 L476JGY. using ESP8266. It doesn't work. How do I do it ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-06-09 10:17 AM
I follow the exact same procedure. I generate code, set GPIO and clock in Cube MX. Open the file in System Workbench. Initialize all the pins right.
I should be connecting the ESP8266 pins to the expansion board right ? This expansion board is connected to the nucleo using the SWD connector.
I feel like I'm missing a step. I ran the example data logger project which works fine on the sensortile.
Labels:
- Labels:
-
GPIO-EXTI
-
STM32L4 series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0