cancel
Showing results for 
Search instead for 
Did you mean: 

How to work LoRa use I-Nucleo-LRWNA1&Nucleo-F746ZG GW (Solve)

PeterChen
Associate

Hi everyone.

I use End-Node example code in I-Cube-LRWAN software to run I-Nucleo-LRWAN1, but my device always say join fail.

I learn to this video step by step do, but also not work.

Conld anyone can help me? Thank you.

Update 2021/11/12

The End-Node example code in I-Cube-LRWAN is not for I-Nucleo-LRWAN expansion board. It's for SX1272MB2DAS expansion board. So if you use I-Nucleo-LRWAN expansion board you only can use LoRaWAN_AT_Master example code in I-Cube-LRWAN.

2 REPLIES 2
Bruno_ST
ST Employee

Hello @PeterChen​ 

There could be multiple reasons for that...

Do you see JOIN packet being catch by the gateway ?

Are you using I-Nucleo-LRWAN1 together with the pack P-NUCLEO-LRWAN2 ?

Did you follow all the steps of the video 2 also ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Do you see JOIN packet being catch by the gateway ?

I see join fail in I-Nucleo-LRWAN1

Are you using I-Nucleo-LRWAN1 together with the pack P-NUCLEO-LRWAN2 ?

Yes.

Did you follow all the steps of the video 2 also ?

Yes.

0693W00000GWwFHQA1.png