2023-04-25 04:14 AM
I am trying to run BLE stack and VCP at the same time but when BLE stack run then VCP disables automatically.
Thank you in advance for reply.
2023-04-25 07:29 AM
+1
I have exactly the same problem right now. Everything is configured in CubeMX and
MX_USB_Device_Init();
is called.
If I comment out
//MX_APPE_Init();
the device is detected as CDC device on the PC.
But if STM32_WPAN is initialized (MX_APPE_Init(); called) the device is not detected as CDC device by the PC: "USB device not recognized"
Edit:
I have tried to narrow down the problem by comment out function calls:
MX_APPE_Init() -> appe_Tl_Init() -> TL_Init()
If I comment out this line in tl_mbox.c, VCP is running (but BLE not):
TL_RefTable.p_device_info_table = &TL_DeviceInfoTable;
Thanks!
2023-04-26 09:31 AM
Hello,
When you call VCP_Init function, a null pointer is give as second parameter, instead this null pointer, give a rx buffer in parameter like this:
VCP_Init( &VcpTxBuffer[0], &VcpRxBuffer[0] );
And declare the rx buffer like this:
static uint8_t VcpRxBuffer[MAX_DBG_TRACE_MSG_SIZE]; /* Receive buffer over USB */
Best Regards
2023-04-26 09:45 PM
Thank you Remy for reply
But in my code CubeMx didn't generate VCP_Init function it generates MX_USB_Device_Init function for usb device (CDC) for virtual com port.
2023-04-26 10:54 PM
hi BGeing.3
Just call this LL_HSEM_1StepLock( HSEM, 5 ); before calling MX_APPE_Init function.
2023-04-27 01:13 AM
Hello,
Sorry, I made a confusion, in your case you can look STM32WB-BLE-USB-CDC-VCOM example available on STM32 Hotspot GitHub. This example demonstrates how to use the BLE component alongside the USB peripheral for point-to-point communications. The application runs the BLE component as a GAP Peripheral and GATT Server, and the USB as a Device Communication Class (CDC), this is a typical application on how to use the STM32WBxx USB Device peripheral where the STM32WB MCU behaves as a USB-to-RS232 bridge following the Virtual COM Port (VCP) implementation.
In AN5289 on figure 9, there is a description that show how to use USB on CPU1 because the USB and RNG IPs share the same source clock, so you should manage semaphore.
Best Regards