Skip to main content
Associate II
February 3, 2025
Question

STM32U575Q CDC USB Device Not Recognized as Virtual COM Port (VCP)

  • February 3, 2025
  • 2 replies
  • 1677 views

Hello everyone,

After successfully built the USB-C PD application with STM32U575Qll + TCPP0203 + BMS. Now I’m trying to establish USB communication between my STM32U575Qll board(USB-C) and Win10(USB2).

I have created the Ux_Device_CDC_ECM project and referenced the example as below:

https://github.com/STMicroelectronics/STM32CubeU5/tree/main/Projects/STM32U575I-EV/Applications/USBX/Ux_Device_CDC_ECM

When the board has been connected to the PC(win10), the Device Manager re-flash when USB2 plug in/out. However, it’s not being recognized as any device in the Device Manager.

I have checked USB-C DP/DM signal level by setting PA11/PA12 as GPIO_OutPut and checked VDDUSB(3.3V), VBUS(5V). I haven't find any hardware issue.

I will be very appreciative if someone could help me on how to solve this problem.

Thanks in advance.

Robert

 

This topic has been closed for replies.

2 replies

ST Technical Moderator
February 5, 2025

Hi @Robert7 

> After successfully built the USB-C PD application with STM32U575Qll + TCPP0203 + BMS.

Would you specify which application Sink Source or DRP? Are you using a reference board? custom PCB? 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Robert7Author
Associate II
February 14, 2025

Hello, 

Thank you for your reply.

The application is STM32U575QII6Q+TCPP0203+BQ25890 custom DRP. TS3USB221RSER has been used for switching USB-C DP_CONN connect to STM32U575QII6Q PA12 and switching USB-C DM_CONN connect to STM32U575QII6Q PA11.

I copied file from: https://github.com/STMicroelectronics/STM32CubeU5/blob/main/Projects/STM32U575I-EV/Applications/USBX/Ux_Device_CDC_ECM/USBX/App/app_usbx_device.c

I have updated 'Main.C', 'app_usbx_device.c', 'app_usbx_device.h' as per Stefanie's Email.

However, it’s still not being recognized as any device in the Device Manager after connecting USB-C DP_CONN, USB-C DM_CONN to USB port of my laptop(win10).

Debug findings:

1) 'app_usbx_device.c' line 201 'if (tx_thread_create...' haven't load 'USBX_APP_Device_Init()'

2) ' _tx_thread_schedule();' run into 'void HardFault_Handler(void)' loop which is from 'tx_thread_schedule.s --> __tx_wait_here:'

 

I don't understand some of the updates on the 'user code' part, and I can't find an example or documentation to explain this. Should I copy all drivers or do something else? I would appreciate it if you could provide application notes, check my attached project, and help me with this.

I attached my zip files.

Thanks.

Best Regards.

Robert