cancel
Showing results for 
Search instead for 
Did you mean: 

How can i fix "Could not determine GDB version using command: " error ?

Selim Sagir
Associate III

Hello,

I am trying to use B-L072Z-LRWAN1 kit with library from Semtech which is Firmware Driver and LoRaWAN Stack V4.1.0. I solved error step by step with adding files one by one. Now that error occurs after Debug program. I am using Ubuntu Disco Dingo.0690X000008AB9nQAG.png

Before this i face with this error when build finished;

 Generate build reports done

arm-atollic-eabi-objcopy.exe -O ihex GPS_Demo.elf GPS_Demo.hex 

Cannot run program "arm-atollic-eabi-objcopy.exe": Unknown reason

Error: Program "arm-atollic-eabi-objcopy.exe" not found in PATH

PATH=[/opt/Atollic_TrueSTUDIO_for_STM32_x86_64_9.3.0/ARMTools/bin:/opt/Atollic_TrueSTUDIO_for_STM32_x86_64_9.3.0/Tools:/home/asus/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin]

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

In my case, I'm more a stable Debian guy. But I made it unstable, my bad. Hence the Kubuntu 23.10 mantic I mentioned.

That Kubuntu lasted ... 5 days, before being so unstable, broken that I went back to Debian ! That resolved the issue, since the libncurses is older under Debian.

 

Also, after a quick look, it seems that the solution by athulmuralidhar below may work