Error Compiling LoRaWAN_End_Node_DualCoreFreeRTOS Example
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-12-03 1:42 AM
Hi all,
I'm reading some code and compiling some examples before receive NUCLEO-WL55JC board.
Problems with this Example: [CM0PLUS]
en.stm32cubewl\STM32Cube_FW_WL_V1.0.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node_DualCoreFreeRTOS
Consola Error:
c:\st\stm32cubeide_1.2.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: LoRaWAN_End_Node_DualCoreFreeRTOS_CM0PLUS.elf section `.text' will not fit in region `ROM'
c:\st\stm32cubeide_1.2.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: region `ROM' overflowed by 7360 bytes
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:69: LoRaWAN_End_Node_DualCoreFreeRTOS_CM0PLUS.elf] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
To try to correct this error, I add optimization (-Os) to reduce the size of the CM0PLUS binary to 68KB (seeing it in the .map, since the size of the binary is 400MB ???).
Best Regards,
Sergio
- Labels:
-
FreeRTOS
-
STM32WL series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-13 8:11 AM
No reactions from the developers of this example yet? I have chosen this MCU because of these FreeRTOS examples.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-13 8:49 AM
Binaries will be large when there are sparse memory sections in the output object file
The developers of the code generally don't participate here, there are a handful of support staff. Most direct engagement is done via local FAE's
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-13 11:32 AM
Well, I have the same Dev board (just arrived and blinks a lot).
My goals are in this order (Note: I am used to NXP Cortex M4 and i.MX CPUs so this may take a bit)
0) Create Dev Environment with STM Tools
1) Compile a Demo
2) Debug Successfully via USB
3) Debug Successfully via Stand Alone J-Link Device
4) Modify code on both cores 'slightly' and recompile and Debug
5) Then do something more meaningful with FreeRTOS and Lora Radio
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-02-26 12:07 PM
I had the same problem and found I could solve it in two ways:
(1) Change from the Debug configuration to the Release configuration (Project > Build Configurations > Set Active)
(2) By changing the compiler optimsation to optimise for size (Properties > C/C++ Build > Settings > MCU GCC Compiler > Optimization select -Os)
I had earlier tried to change the debug settings but that made no difference...
I should say that I don't yet have hardware, so I have not tested this, but it builds.
I would like to understand is the effect of the settings changes. It looks like the system auto-generates makefiles in the Debug and Release folders, but I don't see the optimisation or debug flags there.