cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 triggers multiple NWE for single write in FMC

utku
Associate

Im trying to drive 3.5 inch TFT LCD with STM32H743 using FMC. My setup is :

  • ChipSelect: NE1
  • Memory Type: LCD Interface
  • LCD Register Select: A18
  • Data: 8 Bits

My timing settings are (FMC Clock: 10Mhz): 

  • Address setup time in FMC clock: 3
  • Data setup time in FMC clock: 2
  • Bus Turn around time in FMC clock: 2

Here are the parts of code:

  • #define FMC_BASE ((uint32_t)0x60000000)
  • #define LCD_CMD (*((volatile uint32_t *)(FMC_BASE)))
  • #define LCD_DATA (*((volatile uint32_t *)(FMC_BASE | (1 << 18))))

When I try to write a data, as shown in the attachment, my logic analyzer shows me multiple WR event occured and shows some weird signals on data line (D0-D3).

I do not understand where I did wrong...

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

To drive LCDs through FMC with MCUs with Cortex-M7 you need to configure the LCD memory region in Strongly-Ordered or Device configuration using the MPU.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

To drive LCDs through FMC with MCUs with Cortex-M7 you need to configure the LCD memory region in Strongly-Ordered or Device configuration using the MPU.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.