cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use SMPS in microcontroller for AC-DC converter?

KKIM.6
Senior

The STM32WB55 microcontroller have SMPS internally.

 

Can I use it to convert AC power to DC power for the microcontroller?

 

If possible, I want to supply RF inductive charging power directly to the microcontroller.

 

1 ACCEPTED SOLUTION

Accepted Solutions

it tells you that the minimum input is, essentially, zero - so you can't apply AC.

Therefore you would need to provide any rectification externally.

The datasheet also tells you that it is a step-down SMPS, so it wouldn't be able to cope with a rectified AC supply - which drops to zero once (half-wave) or twice (full-wave) per cycle.

View solution in original post

6 REPLIES 6
KKIM.6
Senior

After reading manual, I understood the SMPS is only for power efficiency when Vdd is high enough than 3.3 V. Unfortunately, I think it cannot be used for AC-DC converter...

"After reading manual, I understood"

Yes, that is why manufacturers provide datasheet to tell you these things!

Absolute Maximum limits:

0693W00000QKdUxQAL.png 

No. My question is whether SMPS in microcontroller can be used for AD-DC converter but, it is not in manual.

Go on.

It clearly tells you that the minimum input is, essentially, zero and the maximum is 4V; so that can't possibly be AC - can it?

0693W00000QKfGEQA1.pnghttps://www.circuitbasics.com/what-is-alternating-current/

Yes. It would be true. However, if there is a diode, I can apply half-wave but still, information is insufficient because I don't know that the SMPS has a bridge rectifier inside.

it tells you that the minimum input is, essentially, zero - so you can't apply AC.

Therefore you would need to provide any rectification externally.

The datasheet also tells you that it is a step-down SMPS, so it wouldn't be able to cope with a rectified AC supply - which drops to zero once (half-wave) or twice (full-wave) per cycle.