2024-07-23 4:47 AM
Hi all
Im using Nucleo WBA52CG development board with STM32Cube FW_WBA V1.4.0
After generating code for BLE using STM32_WPAN i get error ble_wrap.c: No such file or directory
Any help?
Solved! Go to Solution.
2024-08-26 12:16 AM
I have the same problem and unfortunately the workaround doesn't help for me. Anything else I can try? Do you have any forecast for when this will be fixed in STM32CubeMX?
BR
Mattias
2024-08-28 2:49 AM - edited 2024-08-28 2:58 AM
Same problem here, I can confirm the workaround is not working
The new error is
undefined reference to `AHB5_SwitchedOff'
2024-08-28 2:54 AM
For now, the only way is to wait for the Next release of CubeMX and IDE. The only temporary workaround is to roll-back to the previous versions of the STM32CubeMX, IDE and CUBEWBA.
Best Regards
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-29 2:08 AM
I finally got it working with older releases of the programs.
The versions I used are:
STM32CubeIDE 1.14.1
STM32CubeMX 6.10.0
WBA FW 1.2.0
2024-09-20 12:08 AM
Hello,
any news regarding this matter? 2 months already passed.
Best regards
2024-10-01 9:02 AM
Any update on this? I am following the mooc course and I am also getting this error, "fatal error: ble_wrap.c: No such file or directory".
2024-11-17 5:51 PM
I am following the mooc course, too. The versions I used are:
STM32CubeIDE 1.16.1
STM32CubeMX 6.12.1
WBA FW 1.4.1
It's also miss ble_wrap.c file.
I hope this problem can be solved earlier, because my customer hopes to use the WBA55 platform for mass production and shipment in Q1 2025.
2024-12-02 2:04 AM
hello @cvs_dev @Kenwang @HectorV @cvs_dk @massijay
This behavior has been solved on the last version of the STM32CubeMX V6.13.0.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.