cancel
Showing results for 
Search instead for 
Did you mean: 

ble_wrap files missing after cube generation

cvs_dev
Associate II

Hi all

Im using Nucleo WBA52CG development board with STM32Cube FW_WBA V1.4.0

After generating code for BLE using STM32_WPAN i get error  ble_wrap.c: No such file or directory

Any help?

15 REPLIES 15

I have the same problem and unfortunately the workaround doesn't help for me. Anything else I can try? Do you have any forecast for when this will be fixed in STM32CubeMX?

 

BR

Mattias  

massijay
Associate

Same problem here, I can confirm the workaround is not working

The new error is

undefined reference to `AHB5_SwitchedOff'

STTwo-32
ST Employee

Hello @massijay @MattiasH 

For now, the only way is to wait for the Next release of CubeMX and IDE. The only temporary workaround is to roll-back to the previous versions of the STM32CubeMX, IDE and CUBEWBA.

Best Regards

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

massijay
Associate

I finally got it working with older releases of the programs.

The versions I used are:

STM32CubeIDE 1.14.1
STM32CubeMX 6.10.0
WBA FW 1.2.0

cvs_dk
Associate II

Hello,

any news regarding this matter? 2 months already passed.

 

Best regards

HectorV
Associate II

Any update on this? I am following the mooc course and I am also getting this error, "fatal error: ble_wrap.c: No such file or directory".